Manufacturers and research institutes can expect to gain a wide range of benefits by using automation solutions in liquid handling. A dispensing system can precisely fill the wells of large microwell plates in the shortest possible time. Specialists are relieved of repetitive tasks and then have time for value-adding work, such as analysing results or developing new test procedures. In contrast to manual pipetting workflows, the processes are completely standardised. The potential for errors is reduced as each step is carried out using a standardised approach. The closed system creates a clean environment, minimising external disturbances to the cell cultures.
All these factors speak in favour of a high degree of automation for handling cells and tissues, from high-throughput screenings to individual gene therapy analyses and cell culture processes. It is crucial that the process has as little impact on the viability of the cells as possible. Cells vary in size and shape and their concentration in solutions can be different. It is therefore important that parameters such as pressure and opening times can be precisely set and reproduced in automated liquid handling. This enables the loads acting on the cells, such as shear forces and pressure differences, to be monitored and minimised.
In collaboration with Esslingen University of Applied Sciences, Festo has tested the influence of dispensing with the pressure-controlled dispensing system from Festo on cell viability in comparison to pipetting using a manual pipette. Testing with a selected cell line has shown that the average viability of the cells was similar to that of the manually pipetted samples. That means the Festo dispensing system offers a very good basis for gentle and precise handling of cell cultures – with all the advantages of automation. Thanks to the modular design and the ability to adjust the parameters, the system can be adapted to different cell lines and cell concentrations.