End-of-arm tooling

End-of-arm tooling (EOAT) is the essential interface between the robot or handling system and the workpiece. These specialised tools or end effectors are attached to the robot arm, and enable specific tasks such as gripping, joining or testing to be carried out accurately. Without EOAT, robots and handling systems would merely be motion machines without functionality.

It is precisely these tools that provide robots with the ability to perform certain tasks such as gripping parts, connecting components or testing products.

Typical EOAT applications include:

  • Material handling: gripping, lifting and placing components.
  • Machining: drilling, grinding, welding or fastening.
  • Quality inspection: sensor-based monitoring of dimensional accuracy and freedom from defects.

EOAT gives robots the adaptability and efficiency they need to implement complex automation processes. By using specialised tools, a general manipulator becomes a highly customisable system that is precisely tailored to the requirements.

EOAT options: from simple grippers to customised solutions

There are a variety of end-of-arm tools that are used depending on the application and task. The most important are:

Grippers

Grippers are the most commonly used EOATs. They come in various designs, from simple pneumatic or electric grippers consisting of one product to complex grippers for larger components that offer format adjustment to enable flexible gripping. They are suitable for tasks where objects need to be gripped, held and transported to another location. Robot grippers can be flexibly configured to handle objects of different shapes and sizes. These includeprecise force-fit or form-fit grippers such as parallel grippers,vacuum grippers that avoid damaging the workpiece by only gently touching it using suction cups as well asvirtually contactless Bernoulli grippers.

Machining tools

Machining tools include joining tools such as welding guns, riveting tools, screw heads and dosing units for bonding. Machining operations such as drilling, milling or grinding can also be carried out directly with EOATs. This means that the robot can be used not only as a material handling tool, but also as a production machine. They are ideal for ensuring that repetitive processing steps are carried out with a consistent level of quality and safety.

Special solutions

There are numerous special-purpose tools that have been designed for specific tasks. These include sensors for quality control, optical control systems, painting solutions or EOATs for special assembly solutions. Thanks to these special tools, the capabilities of a robot are significantly expanded and they can be used to solve complex tasks efficiently.

The benefits of EOAT: automation, flexibility and cost savings

EOAT offers numerous benefits that are invaluable for automation technology in production:

  • Precision and repetition accuracy: Increase the precision of your automated processes with high-quality end effectors. Gripper robots and machining tools work with millimetre accuracy, making them crucial for high product quality. Choosing the right EOAT is particularly important for applications that require a high level of repetition accuracy.
  • Flexibility: The use of flexible EOATs offers substantial benefits. Robots with modular end effectors can be quickly adapted to new tasks. This means that businesses can flexibly scale or reorganise their production processes without having to put up with major delays. This flexibility is especially useful for businesses that work with changing quantities or product lines.
  • Cost savings: Automation, which is usually only made possible by EOAT, can optimise production processes and reduce labour costs. When robots can be equipped with different end effectors, the utilisation efficiency of the machines is increased and investment costs are reduced in the long term.

However, choosing and integrating EOAT is not without its challenges. The complexity of integrating robots into existing processes and the need to find the right tools for different tasks are important aspects that need to be taken into account. Careful planning is essential to get the full benefit from the end effectors.

Trends and innovations in end-of-arm tooling

End-of-arm tooling technologies are constantly evolving and have a lasting impact on robotics and automation technology. The latest trends include:

  • Collaborative robots (cobots): EOATs for collaborative robots put safety and ergonomics squarely in the foreground. The environment of these cobots is equipped with highly sensitive sensors that enable them to recognise and adapt to obstacles in real time. This makes them ideal for use in factories where people and robots work closely together. That means tools must also be switched off safely if there is a potential hazard. Advances in software integration also improve seamless control and facilitate the integration of EOATs into existing production systems.
  • Artificial intelligence (AI): AI-supported EOATs offer significant advances for automation. They can use machine learning algorithms to optimise their movements, gripping force and task planning based on real-time data and predictions. One application example is the adaptation to different object shapes or weights, providing even greater flexibility. These types of developments help to avoid time-consuming retooling processes or the need for programming when changing tools.
  • Lightweight construction and material innovations: The use of lightweight yet sturdy materials such as carbon fibre and high-performance plastics has significantly improved the efficiency of modern EOATs. These materials not only reduce the energy consumption of robots and handling systems, but also increase their load-bearing capacity and dynamics. At the same time, they simplify the handling and servicing of the tools, which reduces operating costs. These new technologies also improve durability and corrosion resistance, even in demanding environments such as body shops or press shops.

In addition, there are innovative combinations of sensors and gripper technology on the market that are pushing the boundaries of what is feasible in automated material handling. These advances not only make EOATs more efficient, but also more versatile.

Overall Equipment Effectiveness (OEE) is a key metric for indicating the efficiency of production plants. EOATs play an important role in positively influencing the three key factors of OEE: availability, performance and quality.

  • Availability: Flexible EOATs such as modular grippers reduce changeover times and increase machine operating times. Digital monitoring software ensures that potential problems are detected at an early stage and downtime is minimised.
  • Performance: Energy-efficient components for vacuum grippers help to maximise production yield without increasing the strain on resources.
  • Quality: Reliable components for end effectors such as adaptive grippers or sensor solutions ensure consistently correct product quality and minimise rejects.

With the right end effectors, production lines can react more quickly and flexibly to different requirements. EOATs are therefore key for achieving a high OEE and making production efficient and flexible. The correct selection and design of end effectors creates the basis for the successful automation of production lines.

Click here to find out everything you need to know about Overall Equipment Effectiveness (OEE)