In your opinion, what are the biggest costs drives and sources of emission in the manufacturing industry?

Sven Lensdorf: Primary energy costs are certainly the main drivers of rising costs in the manufacturing industry. This is clear, for example, in countries such as Poland, where electricity prices have quadrupled. To offset their CO₂ emissions, companies also have to purchase special certificates, which just goes to show how important an issue this is. In addition, environmental, social and governance issues, known as ESG, require companies to reduce their CO₂ footprint.

What, in your view, are the current challenges when promoting energy efficiency and sustainability in production? And how does Festo meet these challenges?

Sven Lensdorf: A key challenge is raising awareness of energy efficiency, particularly in relation to compressed air. Although compressed air only accounts for a small part of the energy costs, it offers considerable savings potential. Festo addresses this by providing specific advice and training to increase customer awareness and knowledge. Another challenge is closing the gap between the current situation in industry and what is technically possible. Many companies do not realise that their compressed air generation, treatment, distribution and consumption could be improved. This would not only save energy, but also increase the service life of their machines and systems.

To maximise efficiency, we encourage our customers to take a comprehensive approach and look at their entire system. Our aim is to promote an in-depth understanding of compressed air and electric automation so that customers can take the most appropriate measures. The challenges for companies are complex; they include a shortage of resources, capacity problems and, in some cases, a lack of knowledge. Employees are often overloaded with many different tasks and can only concentrate on some of them. Gaps in knowledge in specific areas also contribute to the fact that the required measures are not implemented. Festo sees it as its responsibility to make customers aware of these issues and to support them. One way we do this is through our Festo Energy Saving Services. These allow companies to make significant savings on compressed air systems very quickly.

How do Festo Energy Saving Services contribute to improving energy efficiency in practice?

Sven Lensdorf: Festo Energy Saving Services initially offer transparency about a company's current energy status, whether through meticulous audits or specific sustainability checks. Customers receive quantified data on CO₂ emissions and financial losses, which is crucial to enable them to plan appropriate measures. We then draw up detailed improvement proposals that not only highlight energy savings but also offer practical steps to implement them. In addition, we attach great importance to raising the awareness of our customers' employees and training them. Our aim is to promote a complete learning process that goes beyond the project in question and enables lasting improvements in energy efficiency.

How do your services help companies achieve their ESG goals?

Sven Lensdorf: Our Energy Saving Services aim to raise awareness of the responsible use of resources, especially when it comes to compressed air. We make it clear that compressed air systems really do contribute to CO₂ emissions if they are not operated with renewable energies. A significant proportion of these CO₂ emissions are caused by the use of compressed air. This highlights the responsibility of operators to minimise their CO₂ emissions through effective resource management. Large companies have a decisive influence on the global CO₂ balance, and since CO₂ is a major factor in climate change, they have an important responsibility. We provide support and advice on complying with environmental protection and energy efficiency standards, in particular ISO 50001, with a specific focus on compressed air systems. Our aim is to help customers fulfil their environmental responsibility and achieve sustainable improvements.

Can you explain the added value and impact of Festo Energy Saving Services using a customer example?

Svens Lensdorf: Two years ago, we worked on a project that came about because of a serious leakage problem at the plant of a major automotive supplier. After thoroughly inspecting the plant over a period of four weeks and carrying out the necessary repairs, we were able to reduce the compressed air consumption by almost 20%. This result was achieved without investing in new compressors or structural changes, but through specific improvements on site. Our work showed that even in a highly developed production environment such as Germany, significant savings are possible by focussing on so-called "low-hanging fruit", i.e. measures that can be taken quickly and easily.

How does Festo integrate sustainability and social responsibility into its own operating processes and service offer?

Sven Lensdorf: Sustainability is an integral part of our production and logistics locations, as well as our collaboration with suppliers. We offer a comprehensive catalogue of strategies ranging from the reduction and optimisation of packaging material to the general reduction of resource usage. All with the aim of being CO₂-neutral in Scope 1 and 2 by 2024. To achieve this, we maintain a consistent focus on applying the sustainability principles and services that we also recommend to our customers. We regularly audit our global production sites ourselves, identify weak points and use our Energy Saving Services Portal to boost energy efficiency. In other words, we do exactly what we recommend to others.

To further increase our sustainability efforts, we have joined the Science Based Targets Initiative (SBTi), an alliance of the UNGC, CDP, WWF and WIR. This initiative enables companies to reduce their greenhouse gas emissions using a scientific basis so that the 1.5 °C target of the Paris Agreement can be achieved. By joining, we are committing to regular reviews and transparent reporting of our progress. This commitment also brings significant added value for our customers: we actively support them with planning their energy-efficient solutions and applying them, for example through Festo Energy Saving Services. This helps them to significantly reduce their energy consumption and costs while at the same time pursuing their own sustainability goals more effectively.