Microfluidics is the science and technology of controlling very small amounts of fluid inside tiny channels. These fluids can be liquids or gases, and the channels are often less than a millimetre in width.
At this scale, fluids behave differently. Surface tension, viscosity and channel geometry start to matter more than gravity or turbulence. That gives engineers and scientists a useful advantage: small volumes can be moved, mixed, heated, separated or analysed with a high degree of control.
This is why microfluidics is used in many compact life science devices. It allows a device to manage samples and reagents in a controlled way, often with less space, less fluid and shorter process steps than conventional laboratory setups.
Microfluidics works by guiding fluids through precisely designed microchannels, chambers and control points. Instead of moving a large sample through tubes, a microfluidic device can move tiny amounts of sample and reagent through a compact internal path.
A simple microfluidic process usually includes:
The exact setup depends on the task. A diagnostic device, a dosing system and an organ-on-a-chip model may all use microfluidic principles, but they do not need the same architecture.
Think of a microfluidic chip as a small, structured route for fluids. A sample enters the chip, moves through narrow channels, reaches one or more functional areas and then produces a measurable result. In a lab-on-a-chip system, this route can replace several manual laboratory steps. A single device can help prepare a sample, mix reagents, and control reaction conditions.
The result is a more compact process. Steps that once needed more space, more manual handling and more separate components are becoming shorter and easier to control.
At the microscale, a fluid flow is usually precisely controlled and predictable. In many microfluidic systems, the flow is laminar, which means fluid layers move alongside each other with minimal mixing caused by turbulence. This changes how engineers design a device: Mixing, dosing and reaction timing often depend on channel shape, path length, pressure control and the surface properties of the material.
Three principles are particularly important:
This can be especially valuable for biological and chemical processes. Less sample or reagent volumes may be needed, and sensitive steps can be carried out in a controlled environment.
Microfluidics is used wherever small fluid volumes need to be controlled, analysed or processed. In the life science sector, it is often indispensable in applications where space, sample volume and repeatability are crucial.
Typical application areas include:
If you work on compact life science devices, the following resources can provide further insight into the topic. Our research teams are exploring microfluidic concepts for laboratory automation and medical technology, and how it can be used in areas such as automated CAR-T cell therapy and organ-on-a-chip systems.
Microfluidics is about more than making fluid paths smaller. It is about giving engineers and scientists an effective architecture to precisely control tiny fluid volumes, so compact devices can handle samples, reagents and reactions with maximum efficiency.
The most important points are:
Once the basics are clear, the next useful step is to ask how fluid control can benefit device reliability, repeatability or scale-up.