End-of-arm tooling (EOAT) is the essential interface between the robot or handling system and the workpiece. These specialised tools or end effectors are attached to the robot arm, and enable specific tasks such as gripping, joining or testing to be carried out accurately. Without EOAT, robots and handling systems would merely be motion machines without functionality.
It is precisely these tools that provide robots with the ability to perform certain tasks such as gripping parts, connecting components or testing products.
Typical EOAT applications include:
EOAT gives robots the adaptability and efficiency they need to implement complex automation processes. By using specialised tools, a general manipulator becomes a highly customisable system that is precisely tailored to the requirements.
There are a variety of end-of-arm tools that are used depending on the application and task. The most important are:
Grippers are the most commonly used EOATs. They come in various designs, from simple pneumatic or electric grippers consisting of one product to complex grippers for larger components that offer format adjustment to enable flexible gripping. They are suitable for tasks where objects need to be gripped, held and transported to another location. Robot grippers can be flexibly configured to handle objects of different shapes and sizes. These includeprecise force-fit or form-fit grippers such as parallel grippers,vacuum grippers that avoid damaging the workpiece by only gently touching it using suction cups as well asvirtually contactless Bernoulli grippers.
Machining tools include joining tools such as welding guns, riveting tools, screw heads and dosing units for bonding. Machining operations such as drilling, milling or grinding can also be carried out directly with EOATs. This means that the robot can be used not only as a material handling tool, but also as a production machine. They are ideal for ensuring that repetitive processing steps are carried out with a consistent level of quality and safety.
There are numerous special-purpose tools that have been designed for specific tasks. These include sensors for quality control, optical control systems, painting solutions or EOATs for special assembly solutions. Thanks to these special tools, the capabilities of a robot are significantly expanded and they can be used to solve complex tasks efficiently.
End-of-arm tooling technologies are constantly evolving and have a lasting impact on robotics and automation technology. The latest trends include:
In addition, there are innovative combinations of sensors and gripper technology on the market that are pushing the boundaries of what is feasible in automated material handling. These advances not only make EOATs more efficient, but also more versatile.