How do Festo Energy Saving Services contribute to improving energy efficiency in practice?

Sven Lensdorf: Festo Energy Saving Services initially offer transparency about a company's current energy status, whether through meticulous audits or specific sustainability checks. Customers receive quantified data on CO₂ emissions and financial losses, which is crucial to enable them to plan appropriate measures. We then draw up detailed improvement proposals that not only highlight energy savings but also offer practical steps to implement them. In addition, we attach great importance to raising the awareness of our customers' employees and training them. Our aim is to promote a complete learning process that goes beyond the project in question and enables lasting improvements in energy efficiency.

How do your services help companies achieve their ESG goals?

Sven Lensdorf: Our Energy Saving Services aim to raise awareness of the responsible use of resources, especially when it comes to compressed air. We make it clear that compressed air systems really do contribute to CO₂ emissions if they are not operated with renewable energies. A significant proportion of these CO₂ emissions are caused by the use of compressed air. This highlights the responsibility of operators to minimise their CO₂ emissions through effective resource management. Large companies have a decisive influence on the global CO₂ balance, and since CO₂ is a major factor in climate change, they have an important responsibility. We provide support and advice on complying with environmental protection and energy efficiency standards, in particular ISO 50001, with a specific focus on compressed air systems. Our aim is to help customers fulfil their environmental responsibility and achieve sustainable improvements.

Can you explain the added value and impact of Festo Energy Saving Services using a customer example?

Svens Lensdorf: Two years ago, we worked on a project that came about because of a serious leakage problem at the plant of a major automotive supplier. After thoroughly inspecting the plant over a period of four weeks and carrying out the necessary repairs, we were able to reduce the compressed air consumption by almost 20%. This result was achieved without investing in new compressors or structural changes, but through specific improvements on site. Our work showed that even in a highly developed production environment such as Germany, significant savings are possible by focussing on so-called "low-hanging fruit", i.e. measures that can be taken quickly and easily.

How does Festo integrate sustainability and social responsibility into its own operating processes and service offer?

Sven Lensdorf: Sustainability is an integral part of our production and logistics locations, as well as our collaboration with suppliers. We offer a comprehensive catalogue of strategies ranging from the reduction and optimisation of packaging material to the general reduction of resource usage. All with the aim of being CO₂-neutral in Scope 1 and 2 by 2024. To achieve this, we maintain a consistent focus on applying the sustainability principles and services that we also recommend to our customers. We regularly audit our global production sites ourselves, identify weak points and use our Energy Saving Services Portal to boost energy efficiency. In other words, we do exactly what we recommend to others.

To further increase our sustainability efforts, we have joined the Science Based Targets Initiative (SBTi), an alliance of the UNGC, CDP, WWF and WIR. This initiative enables companies to reduce their greenhouse gas emissions using a scientific basis so that the 1.5 °C target of the Paris Agreement can be achieved. By joining, we are committing to regular reviews and transparent reporting of our progress. This commitment also brings significant added value for our customers: we actively support them with planning their energy-efficient solutions and applying them, for example through Festo Energy Saving Services. This helps them to significantly reduce their energy consumption and costs while at the same time pursuing their own sustainability goals more effectively.