A simple system for reliable solutions

Festo offers a modular system of tried-and-tested components, including miniature cylinders for actuator technology in the smallest of spaces, miniature valves for controlling closely packed channels, and miniature sensors for monitoring the pressure or the position of the lab-on-a-chip.

We design a suitable valve block based on your microfluidic chip layout and select the modules that best meet your specifications. We integrate the components on valve blocks in such a way that the diaphragms on the microfluidic chips are precisely activated. This ensures that the chemicals are transported from the reservoirs into the reaction chambers in exactly the right order, for reliable and reproducible processes.

Festo doesn't just rely on electrical components for the design, but increasingly on pneumatic ones. The highly compact components operate extremely reliably, with minimal heat generation. This is important since the chemicals used are often sensitive to heat. Additional components for cooling can thus be avoided. Built-in pressure and vacuum generation means that no external air supply is necessary.

Controlling the processes in the Festo solutions does not require any complex software. This means the customer does not, for example, have to resort to software of unknown provenance. This eliminates the need for additional checks and avoids potential risks.

Tried-and-tested, certified, and reliably delivered

The jointly developed solutions consist of standard components that Festo, as the global leader in automation technology, can deliver in large quantities in the shortest possible time. The Festo quality management system is certified to ISO 13485. The systems and components are highly reliable thanks to their compliance with the industry standard and have proven themselves in industrial automation. The provisions of the In Vitro Diagnostic Device Regulation (IVDR) have also been taken into account during development.

With Festo as a partner, the quickest route to mass production of a new lab-on-a-chip system is also the most economical and the surest.