Vescon Systemtechnik GmbH is headquartered in Gleisdorf, near Graz, Austria. Here, the company implements a wide range of projects from automation and process engineering right up to power engineering and software development. One of these sophisticated automation and process engineering solutions that was developed specially for the Slovakian plant of Tier 1 supplier ZKW Group, was for the production of full LED headlights. The solution is an LED light module that avoids dazzling other road users thanks to a "matrix arrangement" of the LEDs and the ability to dip individual LED segments, while at the same time ensuring good visibility for the road ahead.
Visual sensors identify the presence of oncoming traffic or vehicles ahead and the segments are selectively switched on or off, depending on the traffic conditions. Coordinated transitions between the light scenarios mean that the driver enjoys a homogeneous and optimized illumination of the road, without that sudden change of light that we are used to when switching from main to dipped beam. The driver's eyes can adjust to the new light setting more easily. This represents an active safety plus because the rest of the surroundings remain well lit by the main beam.
A second, particularly challenging part of the headlight assembly system is the hot riveting. A plastic dome is deformed at a precisely determined temperature to create a rivet head. Christoph Legat: "This rivet head sits on the reflector and it has to hold it and the printed circuit board on the cooling element, completely securely and reliably. The riveting has to be so accurate that no gap can occur, which could cause the components to wobble during the subsequent vibration test or under normal operating conditions. In the worst case, this could impact on the illumination while driving."
The customer opted for a semi-automatic solution where multiple operators are involved. On the one hand, this opened up the opportunity for greater flexibility while keeping costs down. On the other, it made it easier for the manufacturer to take different components or product versions into consideration. In spite of the manual interventions, the complete system is monitored at every step by a controller. Primary control is done through a database that manages all the product data and information relating to the production process of each headlight. At the end of the manufacturing process, each headlight is fully traceable.
As the first step of the process, the operator removes the headlight housing and places it in the processing station. Then the type code or the variant that is to be produced is selected. "A good example is a headlight that is intended for a vehicle that is exported to other, non-European markets. In such cases, other indicator modules are sometimes used because local statutory regulations define that there must be switching between the indicator and the daytime running light," explains Legat.
Each operator works at two or three different assembly stations while locking cylinders ensure that the workpieces are held securely in place. These don't just hold them in place, but in addition, they only release the component once all the necessary processing steps have been carried out correctly. The operator positions the different components and accompanies the headlight until it reaches the first fully automated processing station, the application of the thermal paste. Once it reaches this position, the headlight is already fully wired, and it has been fitted with the adjusting system and the main beam module. Now a turnkey three axis handling system is deployed that was delivered to the Vescon system, by the specialists from the Festo Technical and Application Center.
A ready-to-install handling system ensures the even application of a two-component thermally conductive paste.
The operator places the cooling element (with holes for insertion of the reflectors) in the station and the thermally conductive paste is applied automatically on both sides using the Festo handling system. It always brings the two-component dispensing system to exactly the right position on the right track. In the next step, the printed circuit board with the five LEDS is positioned in the paste on the cooling element. Then the reflectors, with their guide pins to ensure optimum positioning, are applied. Once this is done, the operator removes the complete cooling element and takes it to the next station, where a further Festo handling system takes care of the movement of the rivet head tool.
Here, there are two EGC-80 toothed belt axes with guide slides, synchronized via a connecting shaft and with a space-saving right-angle gear unit (x-axis). There is also a type EGC-HD-160-BS heavy-duty axis with sturdy double guide (y-axis) and a type PLFN flange gear. All axes are equipped with servo actuator packages with multi-turn encoders.
Project Manager Legat is delighted with the ready-to-install handling solutions: "We just gave details of the required characteristics, we defined the loads and the paths or tracks that had to be traveled and then we didn't have to give any more thought to this part. This simplified our work enormously as did being able to use the handling system CAD data that Festo provided us, with for the design of the complete system."