Depending on the programming and the technical equipment, the RoboThespian can actively talk with someone else. His name says it all as ‘Thespian’ is an old English word for an actor. The clever robot speaks several languages and recognizes faces and gestures.

If you say certain key words, it starts with readily defined reactions. It can also use search engines and access information on the Internet independently to give exact answers and advice. If it is controlled by people via a wireless headset and tablet, it can even address visitors individually. There are currently more than 60 of these robots worldwide, mainly in museums, universities or permanent displays, where they delight visitors.

Precise control system using piezo technology

The artificial muscles are controlled among other components by piezo valves VEAB from Festo. They offer numerous benefits compared to conventional solenoid valves, especially in applications for flow and pressure regulation, as well as directly controlled proportional valves. They are very small, lightweight, extremely precise, very durable, switch extremely quickly and require up to 50 per cent less energy. Furthermore, they generate virtually no waste heat and operate almost silently.

Ambassador for Industry 4.0

RoboThespian is a fascinating example of human–machine communication. It is an impressive representation of the future potential of Industry 4.0. People create and program the machine that then reacts largely autonomously and flexibly to its surroundings.

More information about the RoboThespian