The new proportional valve terminal VTEP expands the Controlled Pneumatics product portfolio. It has an impressive and extremely compact multi-channel pressure control with a low flow rate. Up to 5 valves with 10 working channels can be controlled simultaneously with pressure and vacuum. The VTEP is free of copper, nickel and zinc, making it ideal for many industries such as electronics and semiconductors, life science, textiles and battery production.
The variable contact pressure of the individual polishing chambers on the polisher is controlled extremely precisely and ensures excellent polishing results, even when polishing wafers.
Perfect timing in the event of unexpected forces improves process reliability in small and very large web control processes. The VTEP is suitable for the web control of battery foils, for example.
Valves such as the VTEP are also used as pilot valves for media valves. In photolithography, for example, wafers have to be sealed very precisely with a light-resistant coating. A suck-back function ensures that no excess paint escapes.
With the VTEP, it is possible to implement applications such as patch clamping using pressure and vacuum. Paint, adhesives or liquids for testing and analysis, can also be dispensed extremely precisely and according to individual recipes. This is not possible with either electric automation or standard pneumatics.