If the answer is no — or “I’m not sure” — the root issue may be your cylinder specification. Proprietary or non-standard models may seem fine on paper, but when downtime hits, they can become a bottleneck that halts your entire operation.
Let’s look at how standardization protects you before failure strikes.
International Organization for Standardization (ISO) and National Fluid Power Association (NFPA) cylinder standards are brand-agnostic, defining bore sizes, port threads, mounting interfaces and stroke lengths. For example, ISO 15552:2018 profile cylinders specify bore sizes from 32 to 320 millimeters (mm), with standardized mounting options like trunnion mounts and clevis brackets.
These standards mean any cylinder built to the same standard will fit, regardless of the manufacturer. An ISO 15552 cylinder is a true drop-in replacement for any other ISO 15552 unit. The mounting holes align, the ports match and no modifications are required.
When you specify proprietary or non-standardized cylinders, you create supply chain vulnerability:
Interchangeable cylinders eliminate these risks. Since they’re widely stocked and competitively priced across multiple vendors, replacements are typically available the next day.
Beyond fast replacements, standardized cylinders offer long-term operational advantages:
It’s important to distinguish between “cold spec” cylinders and true interchange products. Cold spec cylinders have achieved de facto standard status through widespread use, but they lack guaranteed dimensional compatibility across manufacturers. Slight variations between brands can introduce uncertainty during replacement. True ISO or NFPA cylinders ensure guaranteed interchangeability across multiple manufacturers — no guesswork or compatibility concerns.
The best time to think about cylinder interchangeability is before you face a failure. Whether you’re designing new equipment or reviewing maintenance strategy, standardized cylinders protect you against unexpected downtime.
Download our white paper to explore ISO and NFPA standards and discover how standardized cylinders safeguard your operations. You can also use our online pneumatic sizing and pneumatic simulation tools to select the right interchangeable cylinder for your application.