Drawing circles in the sky. From left to right. Up and down. Completely weightless. As free as a bird. What young and old often dream of can become reality in Burgenland, Austria. A breezy flight at 22 meters (72 feet) above the ground on “Leonardo’s Flying Machine” is just one of many attractions at Familypark in St. Margarethen that makes children’s eyes light up and is lots of fun for the whole family. And the technicians at the amusement park also had fun during an in-house training seminar held by Festo Training and Consulting directly on-site in St. Margarethen. For two days, everything revolved around the topics of pneumatics and electropneumatics – and only marginally on merry-go-rounds. And there are plenty of those at Familypark not far from Lake Neusiedl. Austria’s largest amusement park has around 60 smaller and larger attractions spread over an area of 145,000 square meters (approx. 36 acres).