A number of different products including water, alcohol, glycerine, surfactants, oleic and acetic acids, sodium hydroxide and potassium hydroxide are stored, transported, blended and bottled for the production of car cosmetic products. This requires complex process automation solutions. The Croatian car cosmetics company Alfa Car has taken a big step into the future here. While building a new production plant, the entire production cycle was fully automated, from the raw materials to the bottling line for the finished products. One point of focus was the seamless automation of the process valves.
To address the challenge, the company worked together with the system integrator Arp Lučko and Festo. It would be Festo’s role to project manage the automation of the process valves. To ensure fast integration into the new plant and maximum reliability in the future production process, customized complete solutions were supplied that cover the entire range, from the process valve units to the valve manifolds. When selecting the necessary components, particular attention had to be paid to the explosive environment.
The communication between a large number of different automated ball valves and the new plant's higher-level control system was also decisive for optimum process automation. This requirement was met by a reliable solution with six valve manifolds of type VTUG with a PROFINET bus connection. More than 200 ball valves from different manufacturers can be fully automated in this manner. Using a single source for the ball valve solution took the pressure off both Alfa Car and Arp Lučko when it came to designing and installing the new plant. The extensive coordination of the various process valve suppliers, which Festo handled as part of its project management brief, also made the project easier.
ALFA CAR d.o.o.
Donja Dubrava
Croatia