What is predictive maintenance?

Predictive maintenance is a data-driven maintenance strategy that uses artificial intelligence and sensor technology to predict potential failures before they occur. Instead of relying on fixed maintenance intervals or reacting only after breakdowns, machines and systems are continuously monitored in real time. Relevant data such as vibration, temperature, pressure, or cycle counts, is collected by sensors, analyzed by AI algorithms and transformed into actionable insights.

This approach enables companies to detect anomalies, wear, or creeping deviations at an early stage. For example, pneumatic cylinders, electric drives, or compressors can be monitored permanently, with the system triggering alerts long before a malfunction would cause unplanned downtime. The result: targeted and condition-based maintenance instead of costly, reactive repairs.

In short, predictive maintenance shifts maintenance from a cost factor to a strategic advantage. With AI at the core, manufacturers can boost productivity, reduce risks, and remain competitive in the era of Industry 4.0.

By continuously monitoring the condition of machines and systems, critical events or creeping deviations can be detected at an early stage. Sensors on your machines and systems collect data that is then forwarded to the system or artificial intelligence.

Based on the determined values and calculations, the AI suggests appropriate maintenance and repair measures.

Why companies should rely on AI solutions like predictive maintenance

Increasing (international) competition, rising cost pressures, a massive shortage of skilled labor, and Industry 4.0 are just some of the challenges that manufacturing companies face nowadays. In addition, there are everyday challenges such as the maintenance and servicing of machines and systems.

To remain successful on the market, manufacturing companies must respond quickly and flexibly to changing conditions. Traditional maintenance concepts, such as reactive repairs or fixed maintenance intervals, are no longer sufficient to meet today's challenges. They often lead to unnecessary costs, inefficient use of resources, and unplanned downtimes.

Predictive maintenance offers a clear alternative. By combining sensor data with AI-based algorithms, companies gain real-time insights into the actual condition of machines and components. This enables early detection of anomalies and wear, so that targeted measures can be taken before failures occur. Instead of replacing parts too early or reacting too late, maintenance becomes condition-based and cost-efficient.

The benefits go far beyond preventing downtime. Predictive maintenance helps to extend the service life of machines, reduce spare parts inventories, and optimize personnel deployment. At the same time, energy and material resources are used more efficiently, contributing to sustainability goals.

For companies, this means higher productivity, greater transparency, and a decisive competitive edge. With AI-driven predictive maintenance, manufacturers are not just reacting to problems but actively shaping the future of their production.

Increase OEE: How AI and machine learning enable predictive maintenance in manufacturing

Just one minute of unplanned downtime can cost up to 10,000 euros (in an expensive production facility)! That's 10,000 good reasons to review and optimize outdated maintenance concepts. Especially as most unplanned downtime is caused by the failure of components such as pneumatic cylinders and can be easily avoided through predictive maintenance.

Artificial intelligence is the key enabler of predictive maintenance in manufacturing. While sensors provide the raw data, such as pressure, vibration, or temperature, it is the AI algorithms that uncover hidden patterns and correlations. Machine learning models continuously analyze incoming data streams, compare them with historical values, and identify even the smallest deviations that may indicate wear or failure.

The true strength of AI lies in its ability to learn and adapt. With each cycle, the algorithms become more precise, meaning that predictions improve over time. Instead of simply reacting to alarms, companies receive actionable recommendations: which component is at risk, when it should be serviced, and how downtime can be prevented.

This proactive approach turns maintenance into a strategic tool. Failures are avoided, spare parts can be planned just-in-time, and maintenance resources are deployed exactly where they are needed. This way, AI transforms predictive maintenance from a theoretical concept into a practical, scalable solution that boosts OEE, reduces costs, and increases competitiveness.

Predictive maintenance in practice: monitoring cylinders

Classic tools such as operating or machine data logging have been used for a long time for diagnostics and root cause analysis.

However, they have some disadvantages compared to predictive maintenance:

  • They completely ignore a lot of data and correlations
  • They are far too complex and too expensive in terms of traditional programming
  • They do not provide forward-looking forecasts
  • They do not instigate measures at an early stage

The solution: Festo AX Industrial Apps

With standardized AI apps for predictive maintenance, Festo is making predictive maintenance accessible and scalable for everyone. One of these is Festo AX Motion Insights Pneumatic, the AI app for pneumatic cylinders from all manufacturers. The app immediately detects anomalies and malfunctions in pneumatic drives or the control chain, helping to prevent machine downtime due to component failure. Another app is Festo AX Motion Insights Electric, the plug and play solution for monitoring electric drives.

Festo AX Motions Insights Pneumatic highlights:

  • Continuous monitoring of the pneumatic drive chain for wear and anomalies
  • Connectivity via a PLC
  • Plug-and-play: no data science expertise required
  • Simple display and access using a browser
  • Compatible with drives from all manufacturers: one standard app for everything

Festo AX Motions Insights Electric highlights:

  • Continuous monitoring of the electric drive chain for wear and anomalies
  • Plug and play with CMMT-AS/ST servo drives from Festo
  • No need to intervene via the PLC
  • No data science expertise required
  • Simple display and access using the browser

Conclusion and outlook for Industry 4.0

AI enables predictive maintenance in manufacturing, and with it, a new era of intelligent production. What began as condition monitoring has now become a strategic lever for higher OEE, lower costs, and sustainable resource management. By combining IoT sensor data with machine learning for predictive maintenance, companies not only prevent downtime, but also transform maintenance into a driver of competitiveness.

By integrating AI solutions such as Festo AX Motion Insights Pneumatic into your systems, you can easily improve maintenance and minimize unplanned downtime. AI enables you to optimize your production and the key company metrics.

Looking ahead, predictive maintenance will continue to evolve: AI systems will increasingly be integrated across entire value chains, enabling cross-plant benchmarking, autonomous service planning, and just-in-time spare part logistics. This means that companies that already rely on AI solutions will increase their OEE figures and secure a clear competitive advantage. So what are you waiting for?