First and foremost, liquid handling results depend on reliable measurement results. For example, if there is a large discrepancy between the volume delivered and the volume measured due to poor measurements, this will result in misleading performance metrics. Therefore, it is very important to use appropriate measuring devices. ISO 8655 and ISO 23783 describe various measurement methods and conditions, such as a maximum allowable systematic and random measurement error for different volume ranges. A basic requirement, however, is to keep the ambient conditions as constant as possible and to exclude both external and internal influences.
Even if the measuring devices are order, unsatisfactory results may occur which are not caused by the dispensing or pipetting head. Some typical mistakes and countermeasures are:
As mentioned above, external influences can drastically affect the results. Nevertheless, even small changes to a given dispensing and pipetting head can improve results – especially for small target volumes. Festo uses a pressure-controlled dispensing and pipetting approach. In this case, it is imperative to use a valve with good repeatability and reproducibility without pause time effects. When it comes to dispensing applications, selecting the right needle is also very important.
Let's check this behavior using an example with the Festo VTOE dispensing head. The dispensing results with different needle diameters show two main findings:
Measuring specifications
Looking at the corresponding channel CV values (also called intra-run or intra-assay CV) as a function of the dispensing results of a needle, two other important findings become directly visible:
Measuring specifications
The reason for higher CVs with smaller pulse times is simple: when opening and closing the valves, there are many parameters and properties that can vary slightly (e.g. time resolution of control unit, switching behavior of the valve, liquid flow, etc.). If the pulse time is short, the time portion of switching on and off is higher and thus has a greater influence. This leads to a greater scatter of dispensing results and poorer CVs.
To avoid this, the findings from the first diagram are important. By using a needle with a lower flow rate (e.g. smaller inner diameter), the pulse time can be increased to achieve a certain amount of volume. In this way, the CV values improve again with the same target volume.
In summary, it is obvious that a good liquid handling result depends on several parameters. First of all, suitable measuring equipment is required. In addition, it is very important to avoid external influences by designing suitable fluid channels, creating a clean working atmosphere and keeping the ambient conditions as constant as possible. Finally, by using the right components for each application, internal influences can be eliminated.