Meaning and definition of Remote I/O

Remote I/O or RIO (short for Remote Input/Output), is a system that makes it possible to connect various sensors and actuators at decentralized locations within a system or network, and manage their data via a central controller. Today, Remote I/O is an essential component of modern automation solutions, as it supports the flexible integration and scalable expansion of automation networks. This is particularly important in complex industrial environments in order to manage all the necessary processes efficiently. By integrating Remote I/O, industrial control systems can react flexibly to changes and expansions without the need for major infrastructure changes. By using Remote I/O, companies can reduce their operating costs, increase efficiency and simplify maintenance. Close cooperation with central control units and communication protocols such as PROFINET, EtherCAT or Ethernet/IP is crucial for reliable data transmission and system performance.

How does Remote I/O work?

  • I/O modules: These modules record the signals from sensors (e.g. temperature, pressure sensors) and control actuators (e.g. valves, motors). There are different types of I/O modules, including analog and digital, depending on the type of signals to be processed.
  • Communication interface: The recorded signals are transmitted via a communication interface (e.g., PROFINET, EtherCAT or Ethernet/IP) to the central control system, e.g. a PLC (programmable logic controller). This interface enables bidirectional communication between the Remote I/O modules and the central controller.
  • Bus coupler: The bus coupler connects the I/O modules to the industrial network. It handles communication between the individual modules and the central control unit.

What is the difference between local I/O and Remote I/O?

A local or central I/O is installed in the control cabinet together with the PLC. In contrast, the Remote I/O is installed decentrally and separately from the control unit.

The choice between implementing a local I/O or Remote I/O depends heavily on the individual requirements and framework conditions of an application, e.g. a centralized architecture may make sense in smaller systems, while larger, more complex networks may benefit from the advantages of a decentralized structure. Another aspect that companies should consider is compatibility and integration with existing control systems to ensure a seamless and efficient implementation.

What is distributed I/O?

A distributed I/O is a remote I/O with a predefined and non-expandable number of inputs and outputs. It is not modularly expandable and is a self-contained unit.

Ready for a more efficient automation solution?

Watch our animation to see how modern architectures make your automation simpler, faster and more cost-efficient.​

  • Less cabling – greater performance​
  • Faster communication – increased productivity
  • ​Easy integration – maximum scalability​
Watch the animation and download poster​

Areas of application:

Remote I/O is used in a wide range of industrial and process automation systems to reduce the amount of wiring required. In the chemical and pharmaceutical industries, Remote I/O systems enable precise monitoring of production processes, and thus contribute to compliance with strict safety and quality standards. In the energy and utilities industry, Remote I/O is used in the operation of power plants, water treatment plants and distribution networks. Remote I/O is also used in the automotive industry in larger applications such as production lines and robot cells. Ultimately, the possible applications of Remote I/O are as diverse as the requirements of the various industries, which underlines its importance in modern automation solutions.

High operating costs? Discover your savings potential with our checklist.​

  • Analyze cost factors – uncover hidden cost drivers.​
  • Recognize problems early on – prevent breakdowns and inefficiencies.​
  • Take appropriate measures – optimize and make your processes more efficient.​
Save checklist now​