Developed by the Dutch company Soteria Medical BV, the new Remote Controlled Manipulator (RCM) facilitates the work of doctors and minimises the intensity of the intervention for the patient. The metal-free RCM is used inside the limited space of a magnetic resonance imaging (MRI) scanner.

An important part of the RCM is its sophisticated software system, which is used in conjunction with MRT images for extremely precise needle guide placement. The current images of the target area are compared with previous diagnostic scans. By means of plastic pneumatic motors of the robot, the needle guide to then moved to the exact location. The system is controlled by a Festo valve terminal type MPA. The doctor then guides the biopsy needle safely and accurately to the prostate using MR images to take a tissue sample for further investigation.