Which actuator technology is suitable for your specific automation task?

Selecting the right actuator technology in factory automation is one of the key design decisions. Both pneumatic and electric actuators have proven their worth time and again in a wide variety of applications. However, their operating principles, controllability, and integration effort are fundamentally different.

Therefore, the question "Which actuator technology is better, electric or pneumatic?" cannot be answered in general terms. What matters is not the technology itself, but the task it is intended to fulfill. Those who analyze their requirements thoroughly make more sound decisions.

Why there is no simple answer

Pneumatics works with compressed air as an energy carrier and is particularly suitable for simple, robust motion tasks. Electric actuators use motors and mechanical transmissions, enabling precise, freely programmable movements.

Both technologies are technically mature and reliable. However, their strengths manifest themselves under different conditions. A well-informed decision thus begins with understanding these differences, not with a preference for a specific technology.

Fundamental differences between pneumatics and electrics

  • Pneumatic actuators have an impressively simple design, a low sensitivity to dust, moisture or temperature, and are incredibly sturdy. They are perfect for fast, repetitive movements with clearly defined end positions.
  • Electric actuators, on the other hand, offer high positioning and repeat accuracy. Motion profiles can be flexibly adjusted, forces precisely controlled, and multiple axes synchronized. These characteristics make them highly suitable for complex or varying processes.

Key decision criteria for actuator selection

To make a well-founded selection of actuator technology, it is always important to consider several criteria. Individual aspects such as precision or energy consumption should never be evaluated in isolation; only the interplay of all requirements indicates which solution is technically and economically sensible.

Force, load, and mechanical requirements

The required force and the load to be moved are key influencing factors.

Pneumatic actuators are very suitable for constant loads and clear end positions, such as in clamping or pressing tasks.

Electric actuators demonstrate their strengths when forces need to be variably controlled or precisely reproduced. This is especially relevant for sensitive components or changing product variants.

Speed, dynamics, and motion profiles

Pneumatics is often advantageous for very fast movements with short strokes since pneumatic systems are dynamic and structurally simple.

Electric actuators, on the other hand, enable complex speed and acceleration profiles. Smooth acceleration, controlled braking, and synchronized multi-axis movements can be precisely implemented.

Precision and repeatability

When positions need to be approached precisely or paths need to be followed, electric drive technology is usually the obvious choice. It offers high repeatability and flexible control options.

Pneumatic systems, meanwhile, are ideal when a certain degree of compliance is allowed or even desirable, for example to protect workpieces or for simple handling tasks.

Energy consumption and efficiency

The energy consumption between the two systems differs significantly. While the power consumption of electric actuators can be evaluated directly, in pneumatic systems, the generation and preparation of compressed air also play a role.

A realistic assessment always takes the entire system into account. And, depending on cycle times, standstill phases and holding functions, pneumatics can even offer energy advantages in certain applications.

Economic efficiency and life cycle costs

In addition to investment costs, operating and maintenance costs and spare parts availability are crucial. A seemingly inexpensive solution can prove to be expensive over its life cycle.

Anyone comparing pneumatic and electric systems should therefore always consider the Total Cost of Ownership, i.e., all the costs right from integration to operation.

Typical application profiles in factory automation

Each specific technology has clear application areas.

Pneumatics is frequently found in handling, clamping or pressing tasks that require clear movement sequences.

Electric actuators are increasingly used in applications where high precision is important or those involving flexible product variants or variable processes.

However, this classification is not a fixed rule. Hybrid concepts and new technological developments are continuously expanding the design options.

Pneumatics or electrics in factory automation is not an either/or question. The appropriate actuator technology is based on the requirements of your application, both technically and economically. Those who systematically evaluate criteria such as load, precision, dynamics, environment, and life cycle costs reduce risks and make informed decisions.

White paper “Pneumatics or Electrics in Factory Automation”

Download the white paper “Pneumatics or Electrics in Factory Automation” now

Get a well-structured decision support with comparison tables, practical examples, and a useful actuator selection guide for your automation task.

Download now – Get the guide

Find the right solution faster with digital engineering tools

As well as comparing pneumatic or electric systems, do you also want to have a technically reliable system design? The Festo Engineering Tools help you to systematically check requirements and design actuators, so they fit perfectly, from the first design idea to the actual sizing.

  • Engineering Tools from Festo
    Digital support for selecting, designing, and validating actuator solutions.
  • Pneumatic Simulation
    The design tool for pneumatic applications: Simulation of movements, forces, speeds, and cycle times.
  • Electric Motion Sizing
    The design tool for electric actuators: Sizing of axes, motors and mechanics based on your application data.

Your added value:
You reduce design risks, gain planning certainty, and get a technically and economically suitable solution faster.