Energy losses cannot be reduced reliably if they remain hidden in daily operation. In many production environments data about energy is already collected, but it is often spread across different machines, lines, sensors, and local systems.
This makes it difficult to see where energy is used, where losses occur and which actions should be taken. A line may consume more energy than expected, but without context it is hard to know whether this is caused by normal production demand, idle operation, compressed air leakage, or an inefficient machine state.
Energy monitoring in production creates this visibility. It connects relevant data, makes consumption easier to compare, and helps teams identify abnormal patterns earlier.
The goal is not only to display data. The goal is to turn energy data into a practical basis for action: detect losses, prioritize measures and track whether improvements reduce consumption over time.
In many production environments useful data is already collected, including on energy consumption, compressed air flow, pressure, machine states, or line-level data. But this data is often stored in different systems, or is only available locally. As a result, teams have data points, but no shared overall view.
Energy consumption changes with line speed, machine state, changeovers, idle phases, and production cycles. Without this context, it is difficult to compare usage across lines, machines, or shifts. Teams may see that consumption is high, but not whether it is expected or abnormal.
Energy, maintenance, production, and plant management teams often look at different data. This makes it harder to agree on priorities and act quickly. A shared energy monitoring view provides teams with the same facts so they can discuss and decide which losses should be investigated first.
Energy monitoring becomes more effective when it starts in the right areas. Instead of measuring everything at once, companies should focus on those supply systems, machines or production lines where losses are likely to have the biggest impact.
Typical starting points include:
Look for recurring patterns such as high consumption during idle times, unexpected compressor load, or differences between comparable lines.
An effective starting point combines technical relevance with business values such as cost impact, maintenance effort, frequency of the issue, and potential scalability.
Many companies do not need to start energy monitoring from zero. Flow sensors, pressure sensors, energy meters, PLCs, or machine controllers may already offer really useful data.
The challenge is to combine this data and make it accessible in one shared structure. In complex production environments, one line may contain several machine sections, each with its own data points and interfaces.
When data is isolated, energy consumption can only be viewed locally. Once it is connected, teams can compare consumption across lines, machines, and operating states.
This reduces the effort of a first pilot and makes the approach easier to scale to additional machines, lines or supply systems.
Compressed air losses often become visible as unusual flow, pressure, or consumption patterns. Energy monitoring helps teams detect when demand does not match the expected operating state, for example during idle times, non-productive phases, or after production has stopped.
Not every energy loss is caused by a leak. Higher consumption can also indicate friction, inefficient machine performance, or changing operating conditions. By comparing energy data across similar assets or production states, teams can identify where further investigation is needed.
A high consumption value does not automatically mean there is a problem. It may be linked to production load, machine state, changeovers, or other operating conditions. AI-supported energy monitoring helps teams interpret data in context, so they can distinguish normal demand from abnormal loss patterns.
Visibility only creates value when it leads to action. Once energy losses, unusual consumption patterns or leakage-related anomalies become visible, teams need a clear process to decide what to investigate first.
The most relevant actions are usually those with:
Energy monitoring together with maintenance helps close the loop: Detect an issue, investigate the cause, take corrective action, and verify if consumption has improved.
Over time, this turns energy monitoring into a continuous improvement process. Losses become easier to detect, actions easier to prioritize, and results easier to track.
A pilot should start with one specific question: Which loss should become visible? This could be compressed air leakage, idle consumption, energy use across comparable lines, or inefficiencies in a selected production area. A clear use case keeps the project focused.
The first pilot does not need to cover the entire plant. It is often more effective to start with one line, one device, or one machine group where the expected value is high. This makes it easier to implement measures and evaluate the results.
Before the pilot starts, teams should agree on how success will be measured. Useful metrics include detected losses, reduced manual effort, faster response time, lower consumption, or improved visibility across production areas.
A successful pilot should create more than a one-time dashboard. It should provide a structure that can be extended to additional machines, lines, supply systems, or sites as the value becomes measurable.
Trying to monitor the entire plant from the beginning can make the project complex and difficult to evaluate. A more effective approach is to start with one clear use case, one production area, or one high-consumption supply system.
More data does not automatically lead to betterdecisions. Before gathering data, teams should define what they want to understand or improve, such as compressed air losses, idle consumption, or energy use across comparable lines.
Dashboards only create value when they support everyday tasks. Energy, maintenance, and production teams should be involved early so the monitoring overview reflects real operational issues.
Energy consumption can only be interpreted correctly when it is linked to operating states, production phases, and machine performance. Without this context, teams may confuse normal demand with abnormal losses.
Energy monitoring should not end when the dashboard is live. The real value lies in having a repeatable process: Detect losses, prioritize action, verify improvements, and scale what works.
Energy monitoring creates value when it turns scattered production data into a shared basis for action.