Pneumatic cylinders are components that carry out a movement using compressed air, which is why they are also known as compressed air cylinders. Pneumatic drives are an especially cost-effective solution for a number of application areas – even in extremely tough ambient conditions – and stand out for being really simple to commission. Speeds of between 10 mm/s and 3 m/s can be achieved. Pneumatic cylinders are sturdy and flexible thanks to the compressibility of the air, which also makes them resistant to high external forces.
Pneumatic cylinders are used in numerous applications in automation technology/factory automation. Typical application areas for pneumatic drives are clamping, lifting, countersinking, pushing, pulling, feeding, turning, gripping, clamping and holding, joining, stopping, stamping, embossing and many others.
The range of pneumatic cylinders drives at Festo includes piston rod and rodless cylinders (linear drive), rotary cylinders, tandem, multi-position and stopper cylinders, as well as clamping cylinders, drives with linear guides, and bellows and diaphragm cylinders. As part of the range, we offer many standards-based cylinders with standardised dimensions and mounting interfaces. Cylinders that comply with a specific standard have identical dimensions. There are standards for piston rod cylinders with round design (ISO 6432), compact design (ISO 21287) and for profile and tie rod cylinders (ISO 15552).
In a pneumatic cylinder, the compressed air is used to exert force on a cylinder piston in order move it in a specific direction. The movement of the piston is transferred to the parts to be moved by a piston rod or a frictional connection. A pneumatic cylinder is a drive operated with compressed air usually up to a maximum of 12 bar in order to generate linear or rotary motion. A distinction should be made between single-acting and double-acting cylinders (work is performed only in one direction or in both directions)
Pneumatic cylinders, also called air cylinders, pneumatic actuators, or pneumatic drives, are relatively simple mechanical devices that use the energy of compressed air and turn it into linear motion. Lightweight and low maintenance, pneumatic cylinders generally operate at lower speeds and less force than their hydraulic or electric counterparts, but are a clean and cost-effective option for reliable linear motion in many industrial environments. The most common design consists of a cylinder or tube that is sealed on both ends, with a cap at one end and head at the other end. The cylinder contains a piston, which is attached to a rod. The rod moves in and out of one end of the tube, actuated by compressed air. Two main styles exist: single-acting and double-acting.
Single-acting cylinders are a great choice for applications with space constraints, as these tend to be smaller cylinders than other designs due to their integrated springs that leave less room for compressed air. Analytical equipment, diagnostic instrumentation, bottling machinery, and commercial laundry and kitchen equipment are just a few examples of where these single-acting cylinders are specified. They are typically used in applications where work is performed in one direction. These include tasks such as positioning, marking, clamping, and light assembly.
A double-acting cylinder is a cylinder in which the working fluid acts alternately on both sides of the piston. In order to connect the piston in a double-acting cylinder to an external mechanism, such as a crank shaft, a hole must be provided in one end of the cylinder for the piston rod, and this is fitted with a gland or "stuffing box" to prevent escape of the working fluid. Double-acting cylinders are common in steam engines but unusual in other engine types. Many hydraulic and pneumatic cylinders use them where it is needed to produce a force in both directions. A double-acting hydraulic cylinder has a port at each end, supplied with hydraulic fluid for both the retraction and extension of the piston. A double-acting cylinder is used where an external force is not available to retract the piston or it can be used where high force is required in both directions of travel.
If you are looking for simple, easy-to-use and cheap linear drives, pneumatic cylinder is often the solution. They are sometimes also called air cylinders. The term single-acting pneumatic cylinder refers to the compressed air that exerts a force on only one side of the piston. The compressed air pushes against one side of the piston which is set in motion because of the applied force. The stroke length of single-acting cylinders with integrated spring return is limited by the installed length of the spring. That is why single-acting cylinders are normally made with a maximum stroke length of 50 mm.
Double-acting air cylinders are used when a force has to be applied in both directions. Double-acting cylinders are used when larger stroke lengths are required. A force is generated both during the advancing as well as the retracting stroke of the piston. It is proportional to the compressed air supply pressure and the operational piston surface of the pneumatic cylinder.
In order to detect the piston movement, sensors are used on the cylinders. These are also called position indicators or cylinder sensors. These proximity sensors, which are often magnetic, detect the magnetic field of the piston and activate the switching output.
In addition to linear pneumatic cylinders, there are rotary cylinders for swivel applications. Most rotary cylinders are used for rotations of 90 to 270 degrees. Such as turning products around.
Ordering pneumatic cylinders starts with selecting and configuring the right type. The right type of double-acting or single-acting cylinder can be determined quickly and easily with digital engineering tools.
Web configurators for pneumatic cylinders help when having to choose the right options for the application in question or the industry requirements. Once your shopping cart is full, you can start ordering. Festo pneumatic cylinders and accessories as well as sensors are available worldwide.
In a pneumatic cylinder, the compressed air is used to exert force on a cylinder piston in order move it in a specific direction. The movement of the piston is transferred to the parts to be moved by a piston rod or a frictional connection. A pneumatic cylinder is a drive operated with compressed air usually up to a maximum of 12 bar in order to generate linear or rotary motion. A distinction should be made between single-acting and double-acting cylinders (work is performed only in one direction or in both directions).
A single-acting pneumatic cylinder only has one compressed air connection. The incoming compressed air moves the piston in one direction, and the cylinder force is built up in this direction. If the piston needs to return to its initial position, the air is simply expelled from the cylinder. The mechanical spring pushes the piston back to its initial position. This part has a ventilation/exhaust hole so that no excess or low pressure is generated through the piston movement in the second cylinder chamber.
Benefits:
Disadvantages:
The double-acting cylinder requires compressed air for every direction of movement. On this type of cylinder, the force in both the advancing and retracting direction is built up using compressed air. The simplest way of actuating a double-acting cylinder is by using a 5/2-way valve.
Benefits:
Disadvantages: