BUSKI, the public water supply and sewerage administration company, is responsible for the water supply in the Province of Bursa, in western Turkey. The city where the company is based, Bursa, is Turkey's fourth largest conurbation. Three million people live there with a daily drinking water demand of 700,000 m³. BUSKI goes to great lengths to establish a failure-free water supply system and to build up a functioning infrastructure based on European standards.
In the past, faults in the system could only be determined by on-site maintenance staff. Additionally, chlorine was added to the water at regular intervals, which caused fluctuations in water quality. A further goal of the water treatment modernization project was to achieve energy savings. But this was nothing new for Festo. We have already completely automated and modernized six other water treatment plants in Turkey.
A central element was the modernization and automation of the sand bed filter. You can find out here how we did this. Or you can skip directly to the Festo solution.
BUSKI, the public water supply company was looking for an experienced technology partner to modernize one of its water treatment plants. Through the invitation to tender, they were seeking to achieve five goals:
Systematic automation should increase operational safety. At the same time, the resulting decrease in the consumption of rinsing water and filter sand should reduce the costs of the water treatment. Sensor technology should help the operators to identify faults quickly so that preventative maintenance can ensure seamless operation. And the metering of the germicidal chemicals should be controlled as demand dictates, in order to make the water odorless. Nevertheless, any health risk for the consumers should be kept to a minimum. Targeted training prepared the staff excellently for the efficient operation of the new plant.
Oltre a prodotti e accessori, Festo offre soluzioni complete per la tecnologia dell'acqua. I nostri esperti hanno accompagnato il fornitore d'acqua turco di Bursa dalle prime fasi di pianificazione fino alla formazione dei dipendenti durante il funzionamento.
Insieme a BUSKI, gli esperti Festo hanno preparato un'analisi dei bisogni che ha incluso tutte le stazioni importanti per il processo di trattamento: la vasca del filtro, il dosaggio, la vasca di decantazione, l'ispessitore dei fanghi e la clorazione. Ciò ha portato a un concetto convincente che copriva tutti i requisiti come l'automazione completa, il funzionamento regolare e la facile manutenzione, ma anche le qualifiche dei dipendenti.
I complessivi 28 filtri a sabbia possono essere azionati in modo completamente automatico dopo l'implementazione del concetto: ogni filtro è stato dotato di un nuovo pannello di controllo e di un quadro di comando pneumatico con terminali CPX elettrici modulari. Inoltre, è stato rinnovato il quadro elettrico principale.
Abbiamo sostituito la tecnologia di azionamento obsoleta delle valvole con attuatori pneumatici lineari e rotativi. Anche la rete dell'aria compressa è stata rinnovata e adattata. Ciascun bacino filtrante è ora controllato da isole di valvole.
Un sistema basato sulla piattaforma di automazione CPX garantisce il dosaggio esatto delle sostanze chimiche aggiunte, che adatta automaticamente l'aggiunta alla quantità di acqua che scorre attraverso. Tutti i dati vengono trasferiti al sistema SCADA.
Ciò che prima era laboriosamente fatto a mano è ora curato dal nuovo sistema SCADA, progettato in modo ridondante per la sicurezza dei dati. Controlla l'intero processo e utilizza tutti i dati di processo per creare automaticamente rapporti di stato per la manutenzione preventiva o attività operative. I dipendenti non devono più registrare faticosamente valori come pressione, livello di riempimento, posizioni delle valvole, le date di sostituzione dei filtri o le ore di funzionamento delle pompe. Adesso, invece, puoi leggere ogni parametro centralmente: nella nuova sala di controllo con videowall, il centro SCADA. A tal fine, è stata installata una rete in fibra ottica in tutta la struttura.
Il programma di formazione di Festo Didactic è durato 300 ore e consente ai dipendenti di utilizzare il sistema e i suoi componenti meccatronici o pneumatici in sicurezza. Con questo tipo di formazione, teoria e pratica si completano a vicenda in modo significativo e alla fine i dipendenti ricevono un certificato da Festo.
Inoltre, un esperto della nostra filiale turca è stato sul posto per un anno intero. Si è assicurato che tutto funzionasse senza intoppi nella fase di avvio ed era sempre disponibile a rispondere alle domande. Oggi i meccanici di BUSKI sono in grado di far funzionare e mantenere in modo efficiente il sistema completamente automatizzato. In definitiva, sono loro a garantire il successo del rinnovato impianto di trattamento delle acque di Dobruca.
Il risultato del progetto Dobruca/Bursa è chiaro: il nuovo sistema completamente automatizzato funziona in modo più sicuro, più economico e più efficiente. Il fatto che Festo avesse già lavorato con successo per ISKI, il più grande fornitore di acqua della Turchia, è la prova della nostra esperienza nella tecnologia dell'acqua. La qualità tedesca, il marchio Festo e il concetto di automazione con la pneumatica hanno convinto BUSKI. Implementiamo soluzioni sicure e pulite in un design di sistema semplice con attuatori e valvole facili da utilizzare, mantenere e lavorare in modo affidabile.
In ingegneria, l'esperienza dei nostri colleghi turchi e il supporto offerto sono stati convincenti. Anche i costi relativamente bassi per un impianto completamente automatizzato, il piano di formazione dettagliato e il coaching nel primo anno di attività sono stati argomenti convincenti per i manager BUSKI per scegliere il nostro concetto.
Grazie all'automazione completa, tutti i requisiti BUSKI per il nuovo impianto di lavorazione sono stati soddisfatti. I processi procedurali funzionano in modo affidabile e senza intoppi con i raccordi pneumatici. La qualità dell'acqua è ora notevolmente aumentata, così come l'efficienza nel trattamento dell'acqua. La sabbia filtro e le perdite d'acqua di lavaggio sono state ridotte al minimo. Ultimo ma non meno importante, anche il sapore dell'acqua è notevolmente migliorato. Questa è stata la prima cosa che molti dipendenti hanno notato.
Ammodernamento pneumatico di un sistema di filtraggio a sabbia. Scoprite di nuovo qui, come BUSKI e Festo hanno risolto il problema.