With the help of CAD systems, designers and architects can create and design products and buildings in virtual space. Complex shapes and structures are no longer just in the mind of the designer, but are becoming visible on the screen. However, unusual shapes are like special components that can hardly be produced automatically and are therefore very costly to manufacture. A construction method is needed that will allow a wide variety of designs to be created while at the same time enabling these to be produced cost-effectively.

Flexible and intuitive to operate

This led to the development of parametric CAD systems at the start of the seventies. These were used for constructing machines and vehicles and were mostly intuitive to operate. The product model is no longer saved as a precise geometry. Instead, its shape is stored in the computer as a combination of parameters and numerical variables that specify its size. A cube-shaped object, for instance, is defined by the parameters length, width and height, a cylinder by diameter and height.

Future construction

The digitalization of planning and implementation processes increases economic efficiency. Scripted geometric models are much cheaper than special components produced conventionally. It is possible to reduce the variety of components and to simplify the geometry and the details without having to simplify the overall form. On the contrary, once the models are stored in the computer, the design can be modified directly on the screen by simply changing the numerical values or using a different combination of parameters. The 3D software used is the same as for creating animations.

Bionic Learning Network 3D Cocooner

Digital production: the software transfers the geometry of the structure directly to the parallel kinematic system's motion paths.

Digital production: the software transfers the geometry of the structure directly to the parallel kinematic system's motion paths.