Pneumatic Sizing Release Notes

See what's new in Pneumatic Sizing and what we're gradually rolling out.

Release 12/2022

What's new

  • Entry of value by keyboard for payload, positioning time and tubing length:

Bug fixes

  • Usage of localized decimal and thousand separators
  • Display of prices and units with spaces## Release 07/2022

What's new

  • D-variants of the GRLA have been replaced by VFOE-LE's:

  • Texts/units for the air factor and the cycle time per minute have been changed:

Release 04/2022

What's new

  • See your price of a solution within Pneumatic Sizing:

  • The calculation of air consumption per year was added. Optionally you can change the Compressed air factor according to your environment.

Release 09/2021

What's new

  • New default parameter make more sense (200mm stroke, 10kg payload, 0.6s positioning time)
  • Slider for Payload input now with 0.1kg steps from 0.1kg .. 5kg and with 1kg steps from 5kg .. 100kg
  • Slider for Required positioning time now with steps of 10ms (before 1ms)

Bug fixes

  • Tubing shown as piece (pcs) instead of meter (m)
  • Text in i-buttons too condensed

Release 07/2021

What's new