Sachets

Grabbing a quick bite to eat is a growing trend. Food producers have responded with “convenience” food items. They require packaging machines that can change packaging format very quickly and flexibly, and are capable of metering out quantities of just a few grams with precision. One example is the Sigpack VPF (Vertical Platform Flatpouch).
With this machine, food producers as well as pharmaceutical manufacturers can easily adapt their production to current market conditions. The machine fills up to 1,800 sachets per minute, offering the best performance per square foot of floor space on the market.

Quick adaptation

Thanks to its modular concept, the flat pouch machine is freely scalable from three lanes up to twelve lanes. The number of lanes depends on the required output and pouch sizes. With the new decentralized dosing system, each lane has its own dosing chamber and a stock of product.

“The separation of the feeding devices creates flexibility in a number of areas. Now different products, such as salt and pepper, can be packaged at the same time on one machine,” explained Rolf Steinemann, Product Manager at Bosch Packaging Systems.

Long sealing times at low temperatures guarantee hermetically tight packages, thus ensuring high product quality. The hygienic and ergonomic design makes the Sigpack VPF easy to access, as well as easy to oversee and clean. “Short cleaning and changeover times contribute to high overall equipment effectiveness,” said Steinemann. Precise dosing, deep pouch filling and hermetically tight seams reduce product loss and waste. This makes the packaging process more cost-effective for manufacturers. In particular for the pharmaceutical industry, these qualities contribute greatly to patient safety as over- or under-dosing of powdered medication can be avoided.


Exactly the right dose every time

The filling mechanism is based on an auger dosing system, known for its high degree of accuracy. Intelligent trend control allows readjustment for more precise dosing. “In the first design for the Sigpack VPF we were planning to use the MPA valve manifold from Festo, which would have allowed us to have product feeding per lane with vacuum and compressed air supply while also having two-chamber separation,” explained Maik Lamprecht, Project Manager for the development of the Sigpack VPF.This would have required additional cleaning components and a proportional valve for each lane.

Reliable product distribution

Thanks to the fast activation of new functions via apps, machine developers
only have to create one basic machine type. “We can then quickly and easily select apps and equip machines with different specifications in line with customer requirements,” said Product Manager Rolf Steinemann. In the Sigpack VPF, the “Proportional pressure regulation” app controls the product feeding for the multi-lane dosing process. With changing pouch sizes and powder consistencies, the automation platform ensures reliable product distribution and a dependable feed process.

Individual settings

The additional functions include the adjustable cleaning and ejection pulse. The automation platform monitors the filling process and the valve performance using pressure testing. By monitoring pressure and vacuum, wear and contamination can be detected at an early stage. Leakage control ensures reliable processes with reproducible results. The cleaning and air jet pressure can be set individually for each lane.

“The Festo Motion Terminal makes pneumatics fit for Industry 4.0, as process data from the Festo Motion Terminal can be processed on our own condition monitoring platform,” said Product Manager Rolf Steinemann.

Bosch Packaging Systems AG

Industriestrasse 8
8222 Beringen
Switzerland

Area of business: Development and manufacture of packaging and handling systems for the food, pharmaceutical and other industries.

The head office of the Food division with process and packaging technology is also located in Beringen.