|
Festo Automation Suite - Plug-in
Plug-in for the parameterisation of CPX-AP automation systems
|
1.5.0.215 05/06/2023
|
CommissioningFile and language versions
|
|
Festo Automation Suite - Extension
Parameterization of IO-Link devices connected to a Festo IO-Link master
This installation container adds support for parameterizing of IO-Link devices to Festo Automation Suite. It consists of the IO-Link extension for installing and administering IODDs and the IO-Link plug-in for setting up parameters and retrieving device diagnostics.
|
2.6.0.29 30/05/2023
|
CommissioningFile and language versions
|
|
Festo Automation Suite - Plug-in
Plug-in for the configuration and parametrisation of the servo drive CMMT-ST
New Features: (based on Firmware V033.0.x)
- Mounting position can be parameterized in order to prevent e.g. an axis drop down when using vertical applications
- Additional opportunity to configure the application data on its own page in the navigation tree of the plug-in
- New graphical parameter pages for "Travel to fixed stop" available in order to configure it conveniently
- Renamed parameter page "Jog Mode" to "Manual movement" and new grafic for the Jog-mode in addition
- For a better overview for multi-protocol devices, the relevant parameter pages according to the configured/activated fieldbus are displayed in black font in the navigation tree and not relevant pages appearing light gray (but still configurable).
- Configuration of parallel mounted axes is now also available for ELGA, EGC-TB-xx and ELCC
Fixed Bugs:
- Establishing a connection (via VPN) to the device takes very long time
- Wrong data import from Electric Motion Sizing for drive configuration with gears
- Projects from Handling Guide Online won't be imported correct (partly)
Known Limitation:
- Writable parameters which have been added to the online watchlist are sporadically overwritten on the parameter page.
|
2.6.0.380 24/05/2023
|
CommissioningFile and language versions
|
|
Festo Automation Suite - Plug-in
Plug-in for the configuration and parametrisation of the servo drive CMMT-AS
New Features: (based on Firmware V033.0.x)
- Mounting position can be parameterized in order to prevent e.g. an axis drop down when using vertical applications
- Additional opportunity to configure the application data on its own page in the navigation tree of the plug-in
- New graphical parameter pages for "Travel to fixed stop" available in order to configure it conveniently
- Renamed parameter page "Jog Mode" to "Manual movement" and new graphic for the Jog-mode in addition
- For a better overview for multi-protocol devices, the relevant parameter pages according to the configured/activated fieldbus are displayed in black font in the navigation tree and not relevant pages appearing light gray (but still configurable).
- Configuration of parallel mounted axes is now also available for ELGA, EGC-TB-xx and ELCC
Fixed Bugs:
- Establishing a connection (via VPN) to the device takes very long time
- Wrong data import from Electric Motion Sizing for drive configuration with gears
- Projects from Handling Guide Online won't be imported correct (partly)
Known Limitation:
- Writable parameters which have been added to the online watchlist are sporadically overwritten on the parameter page.
|
2.6.0.380 24/05/2023
|
CommissioningFile and language versions
|
|
Festo Automation Suite - Extension
PLC programming with CODESYS technology
|
2.6.0.93 30/05/2023
|
CommissioningFile and language versions
|
|
Festo Automation Suite
Parameterisation, programming and maintenance of electronic devices by Festo
System Requirements:
- Windows 10 Version 1607 or higher
- Windows 11
- 32 or 64 bit
|
2.6.0.481 30/05/2023
|
CommissioningFile and language versions
|
|
Festo Automation Suite - Plug-in
Plug-in for the parametrisation and diagnosis of the CPX-E automation system and the CPX terminal
|
2.5.0.46 21/12/2022
|
CommissioningFile and language versions
|
|
Festo Automation Suite - Plug-in
Supported systems:
- Proportional-pressure regulator VPPI- (8074287)
|
1.0.0.37 14/04/2022
|
CommissioningFile and language versions
|
|
Festo Automation Suite
Update Container - only for integrated update mechanism
The update container is used by the Festo Automation Suite for its integrated online update mechanism and cannot be installed manually. Please download and install the regular setup file if you want to update an installation on a computer without internet access.
|
1.3.1.57 29/11/2019
|
CommissioningFile and language versions
|
|
Festo Automation Suite - Extension
Extension without CODESYS installation data - only for integrated update mechanism
Already included in the extension for PLC programming with CODESYS technology and is only needed for updates from within the Festo Automation Suite; does not need to be downloaded separately.
|
1.3.0.176 29/11/2019
|
CommissioningFile and language versions
|
|
Festo Automation Suite - Extension
Network scan - only for integrated update mechanism
Already included in the setup of the Festo Automation Suite and does not need to be downloaded and installed separately.
|
1.3.0.537 29/11/2019
|
CommissioningFile and language versions
|
|
EtherCAT XML
EtherCAT XML File for the Servo Drive CMMT-AS-...-EC
Supported systems:
- servo drive CMMT-AS-C12-11A-P3-EC-S1 (8133355)
- servo drive CMMT-AS-C2-11A-P3-EC-S1 (5340821)
- servo drive CMMT-AS-C2-3A-EC-S1 (5340819)
- servo drive CMMT-AS-C3-11A-P3-EC-S1 (5340822)
- servo drive CMMT-AS-C4-3A-EC-S1 (5340820)
- servo drive CMMT-AS-C5-11A-P3-EC-S1 (5340823)
- servo drive CMMT-AS-C7-11A-P3-EC-S1 (8133354)
- Software FESTO AUTOMATION SUITE (8074657)
|
24.0.2.94 23/06/2023
|
Device Description FilesFile and language versions
|
|
PA Toolkit
Supported systems:
- Control block CPX-CEC-C1-V3 (3473128)
- Control block CPX-CEC-M1-V3 (3472765)
- Control block CPX-CEC-S1-V3 (3472425)
- controller CPX-E-CEC-C1 (5226780)
- controller CPX-E-CEC-C1-EP (4252742)
- controller CPX-E-CEC-C1-PN (4252741)
- controller CPX-E-CEC-M1 (5266781)
- controller CPX-E-CEC-M1-EP (4252744)
- controller CPX-E-CEC-M1-PN (4252743)
|
2.0.5.0 17/11/2022
|
Function blocksFile and language versions
|