Description:
Setup for Festo Configuration Tool with CMAX plugIn
- Festo Configuration Tool V1.3.1.1
- CMAX PlugIn V2.3]
- CMAX PlugIn V2.2
- CMAX PlugIn V1.8
- CMAX PlugIn V1.1
- CMAX PlugIn V1.0
Version changes:Version 2.3
Support of new firmware features
- Record list with 128 records[*/]
- Seperated target position and target force in the control data[*/]
- Sign of Life bit[*/]
- Control clamping unit of DGCI externally[*/]
- Secondary actual value transmits error and warning[*/]
Other
- The PlugIn can be used in Japanese language[*/]
- A firmware version can be defined which is to be used for the component[*/]
Supported systems:- Axis controller CPX-CMAX-C1-1 (548932)
- Terminal CPX (197330)