Title:
Festo Automation Suite - Plug-in
Subtitle:
Plug-in for the configuration and parametrisation of the servo drive CMMT-AS
Description:

New Features: (based on Firmware V033.0.x)

  • Mounting position can be parameterized in order to prevent e.g. an axis drop down when using vertical applications
  • Additional opportunity to configure the application data on its own page in the navigation tree of the plug-in
  • New graphical parameter pages for "Travel to fixed stop" available in order to configure it conveniently
  • Renamed parameter page "Jog Mode" to "Manual movement" and new graphic for the Jog-mode in addition
  • For a better overview for multi-protocol devices, the relevant parameter pages according to the configured/activated fieldbus are displayed in black font in the navigation tree and not relevant pages appearing light gray (but still configurable).
  • Configuration of parallel mounted axes is now also available for ELGA, EGC-TB-xx and ELCC


Fixed Bugs:

  • Establishing a connection (via VPN) to the device takes very long time
  • Wrong data import from Electric Motion Sizing for drive configuration with gears
  • Projects from Handling Guide Online won't be imported correct (partly)


Known Limitation:

  • Writable parameters which have been added to the online watchlist are sporadically overwritten on the parameter page.



Document type:
Commissioning
Version Download
Version 2.6.0.380 (24.05.2023)

New Features: (based on Firmware V033.0.x)

  • Mounting position can be parameterized in order to prevent e.g. an axis drop down when using vertical applications
  • Additional opportunity to configure the application data on its own page in the navigation tree of the plug-in
  • New graphical parameter pages for "Travel to fixed stop" available in order to configure it conveniently
  • Renamed parameter page "Jog Mode" to "Manual movement" and new graphic for the Jog-mode in addition
  • For a better overview for multi-protocol devices, the relevant parameter pages according to the configured/activated fieldbus are displayed in black font in the navigation tree and not relevant pages appearing light gray (but still configurable).
  • Configuration of parallel mounted axes is now also available for ELGA, EGC-TB-xx and ELCC


Fixed Bugs:

  • Establishing a connection (via VPN) to the device takes very long time
  • Wrong data import from Electric Motion Sizing for drive configuration with gears
  • Projects from Handling Guide Online won't be imported correct (partly)


Known Limitation:

  • Writable parameters which have been added to the online watchlist are sporadically overwritten on the parameter page.
Version 2.5.1.2 (21.02.2023)

Fixed Bugs:

  • The parameter page "Extended Process Data" is displayed incorrect if PROFINET or EtherNet/IP devices are using.
  • The parameterization of the external brake resistor is being overwritten when enter the page "Device Settings"
  • Incorrect limit calculation (too low) for maximum velocity values of the entire system.
  • The preselected fieldbus configuration from the commissioning file (e.g. HGO, EMS) won't take over to the plug-in.
  • Trace recordings won't be displayed in the correct ordering
Version 2.5.0.761 (15.12.2022)

New Features:

  • Parameter values in the project can be reset to plug-in default values (exceptions: drive configuration, record table and trace channel configuration).
  • Copying, adding and removing of parameter IDs, for example to the trace channel list or watchlist, is now possible directly via a button in the parameter pop-up.

 

Parameter Pages:

  • New parameter page for modulo operation with dynamized graphics in online mode.
  • New diagnostic page for fieldbus process data, which clearly and dynamically displays the current state of the status and control word bits, depending on the used fieldbus and telegram.
  • The byte data structure of the input and output data on the parameter page "Extended process data" can be copied to the function block in the PLC program (Festo-CMMT-PN-Lib).
  • Convenient and size-dependent selection of Festo braking resistors (CACN) on the "Device setting" page.
  • Interactive graphic of the DIL switch setting for the fieldbus setting is displayed on page Fieldbus --> Configuration.

 

Record Table:

  • The velocity override for the configured record sets can be conveniently set via a slider (0-200%) for commissioning.
  • Record sets can be duplicated (right mouse click --> Duplicate) and additionally provided with comments.
  • The executed record set is highlighted with a blue arrow in online mode.

 

Watchlist:

  • Parameters can be sorted as desired within the watchlist by drag-and-drop.
  • All live values in the list can be enlarged and reduced by a slider or via the key combination (CTRL + mouse wheel).


Fixed Bugs:

  • The axis order code for 2D gantries haven't been correct imported from Handling Guide Online (HGO).
  • Establishing a connection to the device, while the servo drive is changing in the configuration, leads to a plug-in crash.
  • Orange warning for the max. velocity has been shown up without visible value changes.
Version 2.4.1.23 (21.09.2022)

New Features:

  • Support of fieldbuses EtherCAT, EtherNet/IP and Modbus-TCP for CMMT-AS-..-MP (Multiprotocol) devices
  • Convenient possibility to apply the recognized servo drive while establishing online connection.


Fixed Bugs:

  • Wrong calculated base velocity value for applications with gear ratio (Application class 4)




Version 2.4.0.464 (24.05.2022)

New Features:

  • Support for CMMT-AS-..-MP (Multiprotocol) devices (only PROFINET)
    • New parameter page “Configuration” to adjust the fieldbus protocol on the device
    • Integration of fieldbus pages for EtherCAT, PROFINET and EtherNet/IP within one plug-in instance
    • New parameter page “Profiles” for parametrization of CiA402 and PROFIdrive profiles
    • Already existing projects (EC, PN, EP) can converted by changing the servo drive to CMMT-AS-..-MP in drive configuration (closed loop data are kept)
    • First setup wizard provides a new TAB “Fieldbus” for fast commissioning
  • Customized watchlist in Online Mode
    • Adding and removing of any parameter ID’s is possible (up to 30)
    • User defined parameter configuration are stored in project folder separately for each device instance
    • Possibility to reset the watchlist parameters to default
  • Import of Handling Guide Online (HGO) commissioning file (incl. closed loop data) for parallel kinematics YXML, YXMF, YXMR (EXCT, EXCH, EXCM)
  • Recommended parameter correction applies automatically after the first configuration in first setup wizard (no orange warnings)
  • Dynamically displaying of relevant parameters (on block or switch) according to the selected homing method on page “Axis”
  • Removing all configured trace channels by clicking one button on page “Trace configuration” is possible


Fixed Bugs:

  • Wrong type description and order code for EMMT-AS-150 and 190er motors in data base
  • Sporadically exception errors and crashes occurs when using trace components
  • Long plug-in loading time when opening, adding, removing or copying a device instance
Version 2.3.0.868 (29.11.2021)

New Features:

  • Drive Configuration
    • Easy and comfortable configuration of parallel axes within the drive configuration and the first setup wizard possible
    • Automatically closed loop calculation for handlings with parallel axes
    • Configuration of mounting kit with gear reduction is possible
  • Parameter pages
    • New parameter page Configuration, below the fieldbus page, for PROFINET and EtherNET/IP devices in order to configure dynamic values in a convenient way
    • A dynamic layout of group AC4 is displaying related to the application basics (linear/rotated) for PROFINET devices
    • Entered feed constant can be taken over for encoder interface 1, 2 and 3 by the selecting "apply for all" in the pop up
    • Automatically saving zero point for multi-turn motors can be activated on parameter page Axis
    • Renamed parameter page "Cam controller" to "Position trigger"


Fixed Bugs:

  • Loading time of the whole parameter list takes very long
  • Wrong importing of the mass inertia for rotate drive from PositioningDrives
  • Stroke limits out of the software limit range leads to a warning during homing
  • Recommended upper and lower thresholds related to the selected supply voltage are offered too low
  • Wrong warnings are shown for EMGA gears in the drive configuration
  • Updating time of the Auto-Tuning results takes too long
Version 2.2.1.4 (16.07.2021)

Fixed Bugs:

  • Valid parameter values from the PositioningDrives engineering tool are overwritten with 0.00 when the file is imported
  • Incorrect incompatibility warning is displayed when using EMMB motors with FW 19.0.4 and Plug-in V2.2.0.1026
Version 2.2.0.1026 (27.05.2021)

New Features:

  • Automatic reading in of the electronic motor type plate when connecting to the device (only for Festo motors with valid EEPROM data).
  • Rapid update of online live values in the parameter list via the button "Refresh".
  • Selection of supply voltage available for 3 phase devices now.
  • Possibility to include additional parameters such as e. g. device name and network settings when exporting a parameter file (pck-file) for the operator unit CDSB.
  • Color for a trace channel can be selected in the context menu on page trace display.
  • Harmonization of trace controls with the topology editor such as e.g. zoom [CTRL + mouse wheel], move diagram [Space + left mouse key], measure X/Y [SHIFT + left mouse key].
  • Incompatibilities between configured components and used target device firmware can be recognized when connecting with the plug-in (e.g. EMMB-AS).
  • Darker device images for improving the contrast in topology editor


Fixed Bugs:

  • Parameter correction leads to invalid parameter values if drive configuration is empty.
  • Exception error when a trace chart image (*.png) is stored on the same local path a second time.
  • The stop signal fails sporadically when jogging via the control panel on page "Manual movement".
  • Memory leak when running several plug-in instances.
  • Recommended value for the velocity limit in positive direction is not applied.
Version 2.1.2.1 (15.02.2021)

Fixed Bugs:

  • Incorrect calculation of recommended limit values for 3-phase devices due to the supply voltage

 

 

Version 2.1.1.11 (26.01.2021)

Fixed Bugs:

  • Save zero point offset after homing is not possible for EMMB-AS motors (FW V19.04.72 absolutely required)
  • Incorrect calculation and updating of parameter "Integral time" on page closed loop

 

 

Version 2.1.0.464 (20.11.2020)

New Features:

  • The predefined feed constant for Festo axes is now adjustable on parameter page "Encoder interface"
  • Separate CODESYS parameter page in the device tree for all CODESYS related settings available (only when connected to a Festo PLC)
  • Homing is possible without enabling the drive, e. g. on current position(requires FW V18 or higher)
  • Executing a record set is possible without enabling the drive, e. g. for changing the parameter set(requires FW V18 or higher)
  • Trace display settings (e. g. grid on/off) now apply to all recordings


Fixed Bugs:

  • Trace display settings (e.g. combined axes, hiding of channels) not stored after leaving the page
  • Software limits not correctly imported from PositiongDrives
  • Warning and error messages are shown for read only parameters
  • The plug-in doesn't reconnect to the device after executing "load factory settings"
  • Trace visualization crashes if it is updated in very short intervals

 

 

Version 2.0.1.8 (28.09.2020)

Fixed Bugs:

  • Error when saving projects (V2.0) with trace settings (trigger type: Diagnostics trigger).
  • Trace overview page loading very slow if many trace results are recorded.

 

 

Version 2.0.0.5 (17.08.2020)

New Features:

  • Support for Festo Automation Suite V2.0
  • New sub page on parameter page "Fieldbus" for CODESYS EtherCAT device settings
  • All released CODESYS driver packages for Point to Point and SoftMotion are included on parameter page "Fieldbus"
  • Master/Slave synchronization for homing can be switched off on parameter page "Encoder interface" (X10 group)


Fixed Bugs:

  • Parameters are resetting to default after toggle measure unit
  • Different information of maximum torque for axes between data base and data sheet

 

 

Version 1.4.0.18 (20.05.2020)

New Features:

  • New Page "Device settings" in first setup wizard
  • Parameter Pages:
    • Improved parameter page "Fieldbus" (includes new sub page "Interface") for PROFINET and EtherNet/IP devices
    • Fieldbus object IDs are shown in parameter pop up window
    • Supply voltage can be selected on parameter page "Device settings"
    • If parameter are not supported by the firmware, only the respective parameter group is disabled instead of the whole page
  • Support for axis and mounting kits
    • EPCC-BS (long stroke) Size 45 and 60
    • EAMM-A-T46 and EAMM-U-87-T46
  • Support for angular gears EMGA-40/60/80-A
  • Support for motors
    • EMMT-AS 60/80/100 with radial shaft seal ring
    • EMMT-AS 60/80/100 with feather key groove (DIN 6885)


Fixed Bugs:

  • Update time of auto tuning results
  • Parameter synchronization dialog erroneously detects differences in parameter values
  • Saving during online session triggers reinitialization of the drive
  • User defined names of record set transitions are not correctly uploaded from the device
  • Warning if an actuator with integrated mounting kit has been imported from PositioningDrives


Included Driver Function Blocks:

  • CODESYS Point to point V3.5.10.47
  • CODESYS SoftMotion V4.0.18.0

 

 

Version 1.3.1.9 (28.02.2020)

Fixed Bugs:

  • Torque, velocity and current limits has been calculated wrong
  • Slow update of live values during online session
  • Wrong velocity limits for axis with intermediate support recommended

 

 

Version 1.3.0.46 (28.11.2019)

New Features:

  • Support for CMMT-AS-C7-... and CMMT-AS-C12-...
  • Support for master/slave mode
  • Support for vibration compensation
  • Device connection:
    • Automatically reconnect after device restart
    • Immediate notification if device connection is lost
  • Parameter and control pages:
    • Block diagrams as alternative view for selected parameter pages
    • Encoder parameterisation for user defined motors now on parameter page "Encoder interface"
    • Calculation of system limits for user defined components
    • Calculation of closed loop parameters possible in online mode
    • Configuration of the X10 interface
    • Teaching of current torque in feed forward control (for vertical axes)
    • Responsive design for control page "Manual movement"
  • Trace improvements:
    • New trace data is read from the device automatically
    • User defined channels
    • Trace start is possible in undocked window
  • PositioningDrives import includes supply voltage


Fixed Bugs:

  • Sporadic problems when importing form EtherCAT scan
  • Modified device name is not stored after "store on device"
  • PROFINET IP address is only shown after reloading the parameter list
  • Integrated mounting kit is not updated after changing the size
  • Auto tuning wizard does not calculate start parameters
  • Incorrect warning messages raised by parameter correction
  • Window area "manual movement" is cut up after zooming


Included Driver Function Blocks:

  • CODESYS Point to point V3.5.10.44
  • CODESYS SoftMotion V4.0.16.0

 

 

Version 1.2.2.4 (02.10.2019)

Fixed Bugs:

  • Calculated limits for current and torque too low for systems with spindle axes

 

Included Driver Function Blocks:

  • CODESYS Point to point V3.5.10.40
  • CODESYS SoftMotion V4.0.16.0

 

 

Version 1.2.1.19 (21.08.2019)

New Features:

  • Support for CMMT-AS-...-EP with Ethernet/IP interface


Fixed Bugs:

  • Exception when entering certain feed constants
  • Error when synchronizing string parameters with the device
  • Text on button for releasing the holding brake not unreadable
  • Reinit after changing the hardware switch settings not possible
  • SoftMotion driver version not displayed
  • User defined gear is deleted when changing the axis
  • Zero point offset is not stored correctly in certain cases
  • Reinit icons missing for some parameters
  • Exception when editing an existing drive configuration
  • Missing scroll bars on page Diagnosis -> I/O state


Included Driver Function Blocks:

  • CODESYS Point to point V3.5.10.38
  • CODESYS SoftMotion V4.0.16.0

 

 

Version 1.2.0.25 (11.06.2019)

New Features:

  • Support for PositioningDrives data import
  • Support for cam controller function (position trigger)
  • Support for touch probe function
  • Parameter export to CDSB operator unit
  • Calculation of system limits:
    • Warnings are shown if parameter values exceed calculated limits
    • Dialog for resetting inconsistent parameters to recommended values
  • First setup wizard:
    • Supply voltage selection
    • Consistency check for homing method and hardware switches
  • Parameter pages:
    • Order of contexts "Control" and "Diagnosis" changed
    • Warnings on parameter pages are indicated in navigator
    • Device details can be displayed on drive configuration page
    • Consistency check for digital I/Os
    • Simplified encoder settings
    • Consistency check for homing method and hardware switches
    • Software limits can be teached
  • Trace improvements:
    • Multiple signals can be selected when adding a trace channel
    • Masking of individual bits for trace channels and trigger
    • Possibility to share Y axis for signals
    • Improved handling of several trace records


Fixed Bugs:

  • Exception when entering certain feed constants
  • Error when synchronizing string parameters with the device
  • Text on button for releasing the holding not unreadable
  • Reinit after chaning the hardware switch settings not possible
  • SoftMotion driver version not displayed
  • User defined gear is deleted when chaning the axis
  • Zero point offset is not stored correctly in certain cases
  • Reinit icons missing for some parameters
  • Exception when editing an existing drive configuration
  • Missing scroll bars on page Diagnosis -> I/O state


Included Driver Function Blocks:

  • CODESYS Point to point V3.5.10.34
  • CODESYS SoftMotion V4.0.14.0

 

 

Version 1.1.1.8 (03.04.2019)

New Features:

  • Updated online help (V1.1.1)
  • Support for CMMT-AS with PROFINET interface
  • Performance improvements (loading, drive configuration page, connecting to a device, parameter synchronization)
  • Online access to user documentation for configured drive components
  • Completely revised trace functionality (better usability, more functions)
  • Improved trace configuration
  • Graphical display of the last autotuning result (requires firmware V15 or higher)
  • Operating mode can be displayed in monitored values
  • Warning in case of implausible software limits
  • Warning when disconnecting from the device if parameters have not been stored permanently
  • Calculated inertia ratio is displayed at the closed loop parameters
  • Improved handling of closed loop parameter sets
  • Improved indication of new trace recording, required restart and required reinitialization
  • Improved toolbar behaviour when reducing the window size
  • Double-clicking in a pop-up directly applies the selected list entry


Fixed Bugs:

  • User defined gear is deleted under certain circumstances (V1.1.1)
  • Version of SoftMotion driver is not displayed correctly (V1.1.1)
  • PROFINET MAC and IP address is not formatted correctly (V1.1.1)
  • Diagnosis page "I/O state" is updated sluggishly
  • User defined settings for auto tuning are not applied
  • Overall gear ratio is not calculated correctly
  • Parameter synchronization dialog is empty in some cases
  • Sorting of error messages via their category does not work properly (page "Error classification")
  • High memory consumption when accessing many parameter pages
  • Trace recording can only be read if the Plug-in is connected to the device when the trigger fires
  • Record list is not copied correctly when copying and pasting a device
  • Error log is not sorted correclty


Included Driver Function Blocks:

  • CODESYS Point to point V3.5.10.30
  • CODESYS SoftMotion V4.0.14.0


 

Version 1.1.0.110 (28.01.2019)

New Features:

  • Support for CMMT-AS with PROFINET interface
  • Performance improvements (loading, drive configuration page, connecting to a device, parameter synchronization)
  • Online access to user documentation for configured drive components
  • Completely revised trace functionality (better usability, more functions)
  • Improved trace configuration
  • Graphical display of the last autotuning result (requires firmware V15 or higher)
  • Operating mode can be displayed in monitored values
  • Warning in case of implausible software limits
  • Warning when disconnecting from the device if parameters have not been stored permanently
  • Calculated inertia ratio is displayed at the closed loop parameters
  • Improved handling of closed loop parameter sets
  • Improved indication of new trace recording, required restart and required reinitialization
  • Improved toolbar behaviour when reducing the window size
  • Double-clicking in a pop-up directly applies the selected list entry


Fixed Bugs:

  • Diagnosis page "I/O state" is updated sluggishly
  • User defined settings for auto tuning are not applied
  • Overall gear ratio is not calculated correctly
  • Parameter synchronization dialog is empty in some cases
  • Sorting of error messages via their category does not work properly (page "Error classification")
  • High memory consumption when accessing many parameter pages
  • Trace recording can only be read if the Plug-in is connected to the device when the trigger fires
  • Record list is not copied correctly when copying and pasting a device
  • Error log is not sorted correclty


Included Driver Function Blocks:

  • CODESYS Point to point V3.5.10.29:
    • Significant improvements for buffered motion tasks
    • Various bug fixes, especially concerning halt and stop actions
    • New parameters "Active" and "ContinuousUpdate" for movement function blocks
    • New property "SetpointAcknowledge"
  • CODESYS SoftMotion V4.0.14.0:
    • unchanged


Supported Systems:

  • Servo Drive CMMT-AS-C2-3A-EC-S1 (5340819)
  • Servo Drive CMMT-AS-C4-3A-EC-S1 (5340820)
  • Servo Drive CMMT-AS-C2-3A-PN-S1 (5340814)
  • Servo Drive CMMT-AS-C4-3A-PN-S1 (5340815)
Version 1.0.2.5 (20.09.2018)

New Features:

  • First release

 

Supported Systems:

  • Servoantriebsregler CMMT-AS-C2-3A-EC-S1 (5340819)
  • Servoantriebsregler CMMT-AS-C4-3A-EC-S1 (5340820)

 

Version 1.0.1.10 (19.07.2018)

New Features:

  • Online help now includes the device manual

 

Fixed Bugs:

  • Several stabilisation improvements
  • Wrong I2t-settings for Festo motors
  • No user prompt when components are deleted in drive configuration
  • Error when transferring parameters from Auto Tuning results
  • Application mass is not applied in closed loop parameter sets
  • Reading a trace recording from the device is not possible if the trigger fired while the plug-in was offline
  • Record list data is not transferred correctly if a device is copied in Designer

 

Supported Systems:

  • Servo Drive CMMT-AS-C2-3A-EC-S1 (5340819)
  • Servo Drive CMMT-AS-C4-3A-EC-S1 (5340820)
Version 1.0.0.45 (07.06.2018)

New Features:

  • First release

 

Supported Systems:

  • Servoantriebsregler CMMT-AS-C2-3A-EC-S1 (5340819)
  • Servoantriebsregler CMMT-AS-C4-3A-EC-S1 (5340820)