|
Version 2.6.0.380 (24.05.2023)
New Features: (based on Firmware V033.0.x)
- Mounting position can be parameterized in order to prevent e.g. an axis drop down when using vertical applications
- Additional opportunity to configure the application data on its own page in the navigation tree of the plug-in
- New graphical parameter pages for "Travel to fixed stop" available in order to configure it conveniently
- Renamed parameter page "Jog Mode" to "Manual movement" and new grafic for the Jog-mode in addition
- For a better overview for multi-protocol devices, the relevant parameter pages according to the configured/activated fieldbus are displayed in black font in the navigation tree and not relevant pages appearing light gray (but still configurable).
- Configuration of parallel mounted axes is now also available for ELGA, EGC-TB-xx and ELCC
Fixed Bugs:
- Establishing a connection (via VPN) to the device takes very long time
- Wrong data import from Electric Motion Sizing for drive configuration with gears
- Projects from Handling Guide Online won't be imported correct (partly)
Known Limitation:
- Writable parameters which have been added to the online watchlist are sporadically overwritten on the parameter page.
|
CMMT-ST_2.6.0.380.fsi
Deutsch [de], English [en]
File size: 167 MB
Version: 2.6.0.380 (24/05/2023)
|
|
Version 2.5.1.2 (21.02.2023)
Fixed Bugs:
- The parameter page "Extended Process Data" is displayed incorrect if PROFINET or EtherNet/IP devices are using.
- Incorrect limit calculation (too low) for maximum velocity values of the entire system.
- Trace recordings won't be displayed in the correct ordering
|
CMMT-ST_2.5.1.2.fsi
Deutsch [de], English [en]
File size: 154 MB
Version: 2.5.1.2 (21/02/2023)
|
|
Version 2.5.0.761 (15.12.2022)
New Features:
- Support for CMMT-ST-C8-1C-MP-S0 (Multiprotocol) device
- New parameter page “Configuration” to adjust the fieldbus protocol on the device
- Integration of fieldbus pages for EtherCAT, PROFINET and EtherNet/IP within one plug-in instance
- New parameter page “Profiles” for parametrization of CiA402 and PROFIdrive profiles
- Already existing projects (EC, PN, EP) can converted by changing the servo drive to CMMT-AS-..-MP in drive configuration (closed loop data are kept)
- First setup wizard provides a new TAB “Fieldbus” for fast commissioning
- Parameter values in the project can be reset to plug-in default values (exceptions: drive configuration, record table and trace channel configuration).
- Copying, adding and removing of parameter IDs, for example to the trace channel list or watchlist, is now possible directly via a button in the parameter pop-up.
Parameter Pages:
- New parameter page "Energy Recovery" with graphical support for adjust setting of the energy load.
- New parameter page for modulo operation with dynamized graphics in online mode.
- New diagnostic page for fieldbus process data, which clearly and dynamically displays the current state of the status and control word bits, depending on the used fieldbus and telegram.
- The byte data structure of the input and output data on the parameter page "Extended process data" can be copied to the function block in the PLC program (Festo-CMMT-PN-Lib).
- Interactive graphic of the DIL switch setting for the fieldbus setting is displayed on page Fieldbus --> Configuration.
Record Table:
- The velocity override for the configured record sets can be conveniently set via a slider (0-200%) for commissioning.
- Record sets can be duplicated (right mouse click --> Duplicate) and additionally provided with comments.
- The executed record set is highlighted with a blue arrow in online mode.
Watchlist:
- Parameters can be sorted as desired within the watchlist by drag-and-drop.
- All live values in the list can be enlarged and reduced by a slider or with the key combination (CTRL + mouse wheel).
Fixed Bugs:
- The axis order code for 2D gantries haven't been correct imported from Handling Guide Online (HGO).
- Establishing a connection to the device, while the servo drive is changing in the configuration, leads to a plug-in crash.
- Orange warning for the max. velocity has been shown up without visible value changes.
|
CMMT-ST Plug-in_2.5.0.761.fsi
Deutsch [de], English [en]
File size: 154 MB
Version: 2.5.0.761 (15/12/2022)
|
|
Version 2.4.1.23 (21.09.2022)
New Features:
- Convenient possibility to apply the recognized servo drive while establishing online connection.
Fixed Bugs:
- Wrong calculated base velocity value for applications with gear ratio (Application class 4)
|
CMMT-ST_2.4.1.23.fsi
Deutsch [de], English [en]
File size: 147 MB
Version: 2.4.1.23 (21/09/2022)
|
|
Version 2.4.0.464 (24.05.2022)
New Features:
- Support for CMMT-AS-..-MP (Multiprotocol) devices (only PROFINET)
- New parameter page “Configuration” to adjust the fieldbus protocol on the device
- Integration of fieldbus pages for EtherCAT, PROFINET and EtherNet/IP within one plug-in instance
- New parameter page “Profiles” for parametrization of CiA402 and PROFIdrive profiles
- Already existing projects (EC, PN, EP) can converted by changing the servo drive to CMMT-AS-..-MP in drive configuration (closed loop data are kept)
- First setup wizard provides a new TAB “Fieldbus” for fast commissioning
- Customized watchlist in Online Mode
- Adding and removing of any parameter ID’s is possible (up to 30)
- User defined parameter configuration are stored in project folder separately for each device instance
- Possibility to reset the watchlist parameters to default
- Import of Handling Guide Online (HGO) commissioning file (incl. closed loop data) for parallel kinematics YXML, YXMF, YXMR (EXCT, EXCH, EXCM)
- Recommended parameter correction applies automatically after the first configuration in first setup wizard (no orange warnings)
- Dynamically displaying of relevant parameters (on block or switch) according to the selected homing method on page “Axis”
- Removing all configured trace channels by clicking one button on page “Trace configuration” is possible
Fixed Bugs:
- Wrong type description and order code for EMMT-AS-150 and 190er motors in data base
- Sporadically exception errors and crashes occurs when using trace components
- Long plug-in loading time when opening, adding, removing or copying a device instance
|
CMMT-ST_2.4.0.464.fsi
Deutsch [de], English [en]
File size: 141 MB
Version: 2.4.0.464 (24/05/2022)
|
|
Version 2.3.0.868 (29.11.2021)
New Features:
- Drive Configuration
- Easy and comfortable configuration of parallel axes within the drive configuration and the first setup wizard possible
- Automatically closed loop calculation for handlings with parallel axes
- Configuration of mounting kit with gear reduction is possible
- Parameter pages
- New parameter page Configuration, below the fieldbus page, for PROFINET and EtherNET/IP devices in order to configure dynamic values in a convenient way
- A dynamic layout of group AC4 is displaying related to the application basics (linear/rotated) for PROFINET devices
- Renamed parameter page "Cam controller" to "Position trigger"
Fixed Bugs:
- Loading time of the whole parameter list takes very long
- Wrong imported mass inertia for rotative drives from PositioningDrives
- Stroke limits out of the software limit range leads to a warning during homing
- Recommended upper and lower thresholds related to the selected supply voltage are offered too low
- Wrong warnings are shown for EMGA gears in the drive configuration
- Updating time of the Auto-Tuning results takes too long
|
CMMT-ST_Plug-in_2.3.0.868.fsi
Deutsch [de], English [en]
File size: 141 MB
Version: 2.3.0.868 (29/11/2021)
|
|
Version 2.2.1.4 (16.07.2021)
Fixed Bugs:
- Valid parameter values from the PositioningDrives engineering tool are overwritten with 0.00 when the file is imported
|
CMMT-ST Plug-in_2.2.1.4.fsi
Deutsch [de], English [en]
File size: 133 MB
Version: 2.2.1.4 (16/07/2021)
|
|
Version 2.2.0.1026 (27.05.2021)
New Features:
- Rapid update of online live values in the parameter list via the button "Refresh".
- Color for a trace channel can be selected in the context menu on page trace display.
- Harmonization of trace controls with the topology editor such as e.g. zoom [CTRL + mouse wheel], move diagram [Space + left mouse key], measure X/Y [SHIFT + left mouse key].
- Incompatibilities between configured components and used target device firmware can be recognized when connecting with the plug-in.
- Darker device images for improving the contrast in topology editor
Fixed Bugs:
- Parameter correction leads to invalid parameter values if drive configuration is empty.
- Exception error when a trace chart image (*.png) is stored on the same local path a second time.
- Cable length and cable cross section is set to default values when resetting the closed loop data.
- The stop signal fails sporadically when jogging via the control panel on page "Manual movement".
- Memory leak when running several plug-in instances.
- Recommended value for the velocity limit in positive direction is not applied.
|
CMMT-ST Plug-in_2.2.0.1026.fsi
Deutsch [de], English [en]
File size: 133 MB
Version: 2.2.0.1026 (27/05/2021)
|
|
Version 2.1.1.11 (26.01.2021)
Fixed Bugs:
- Incorrect calculation and updating of parameter "Integral time" on page closed loop.
|
CMMT-ST Plug-in_2.1.1.11.fsi
Deutsch [de], English [en]
File size: 119 MB
Version: 2.1.1.11 (26/01/2021)
|
|
Version 2.1.0.464 (20.11.2020)
New Features:
- The predefined feed constant for Festo axes is now adjustable on parameter page "Encoder interface"
- Separate CODESYS parameter page in the device tree for all CODESYS related settings available (only when connected to a Festo PLC)
- Homing is possible without enabling the drive, e. g. on current position(requires FW V18 or higher)
- Executing a record set is possible without enabling the drive, e. g. for changing the parameter set(requires FW V18 or higher)
- Trace display settings (e. g. grid on/off) now apply to all recordings
Fixed Bugs:
- Trace display settings (e.g. combined axes, hiding of channels) not stored after leaving the page
- Software limits not correctly imported from PositiongDrives
- Warning and error messages are shown for read only parameters
- The plug-in doesn't reconnect to the device after executing "load factory settings"
- Trace visualization crashes if it is updated in very short intervals
|
CMMT-ST Plug-in_2.1.0.464.fsi
Deutsch [de], English [en]
File size: 119 MB
Version: 2.1.0.464 (20/11/2020)
|
|
Version 2.0.1.8 (28.09.2020)
Fixed Bugs:
- Error when saving projects (V2.0) with trace settings (trigger type: Diagnostics trigger).
- Trace overview page loading very slow if many trace results are recorded.
|
CMMT-ST Plug-in_2.0.1.8.fsi
Deutsch [de], English [en]
File size: 108 MB
Version: 2.0.1.8 (28/09/2020)
|
|
Version 2.0.0.5 (17.08.2020)
New Features:
- Support for Festo Automation Suite V2.0
- New sub page on parameter page "Fieldbus" for CODESYS EtherCAT device settings
- All released CODESYS driver packages for Point to Point and SoftMotion are included on parameter page "Fieldbus"
Fixed Bugs:
- Modified parameters of intermediate circuit voltage will be overwritten automatically by saving the project.
- Parameters are resetting to default after toggle measure unit
- Different information of maximum torque for axes between data base and data sheet
|
CMMT-ST Plug-in_2.0.0.5.fsi
Deutsch [de], English [en]
File size: 114 MB
Version: 2.0.0.5 (17/08/2020)
|
|
Version 1.4.0.18 (20.05.2020)
New Features:
- New Page "Device settings" in first setup wizard
- Selection of supply voltage 24V/48V possible
- Parameter Pages:
- Improved parameter page "Fieldbus" (includes new sub page "Interface") for PROFINET and EtherNet/IP devices
- Fieldbus object IDs are shown in parameter pop up window
- Supply voltage can be selected on parameter page "Device settings"
- If parameter are not supported by the firmware, only the respective parameter group is disabled instead of the whole page
- Support for axis and mounting kits
- EPCC-BS (long stroke) Size 45 and 60
- EAMM-A-T46 and EAMM-U-87-T46
- Support for angular gears EMGA-40/60/80-A
Fixed Bugs:
- Update time of auto tuning results
- Parameter synchronization dialog erroneously detects differences in parameter values
- Saving during online session triggers reinitialization of the drive
- User defined names of record set transitions are not correctly uploaded from the device
- Warning if an actuator with integrated mounting kit has been imported from PositioningDrives
Included Driver Function Blocks:
- CODESYS Point to point V3.5.10.47
- CODESYS SoftMotion V4.0.18.0
|
CMMT-ST_1.4.0.18.fsi
Deutsch [de], English [en]
File size: 52 MB
Version: 1.4.0.18 (20/05/2020)
|
|
Version 1.3.1.9 (28.02.2020)
Fixed Bugs:
- Torque, velocity and current limits has been calculated wrong
- Slow update of live values during online session
- Wrong velocity limits for axis with intermediate support recommended
|
CMMT-ST_1.3.1.9.fsi
Deutsch [de], English [en]
File size: 49 MB
Version: 1.3.1.9 (28/02/2020)
|
|
Version 1.3.0.46 (28.11.2019)
New Features:
- Support for vibration compensation
- Device connection:
- Automatically reconnect after device restart
- Immediate notification if device connection is lost
- Parameter and control pages:
- Block diagrams as alternative view for selected parameter pages
- Encoder parameterisation for user defined motors now on parameter page "Encoder interface"
- Calculation of system limits for user defined components
- Calculation of closed loop parameters possible in online mode
- Teaching of current torque in feed forward control (for vertical axes)
- Responsive design for control page "Manual movement"
- Trace improvements:
- New trace data is read from the device automatically
- User defined channels
- Trace start is possible in undocked window
Fixed Bugs:
- Modified device name is not stored after "store on device"
- PROFINET IP address is only shown after reloading the parameter list
- Integrated mounting kit is not updated after changing the size
- Auto tuning wizard does not calculate start parameters
- Incorrect warning messages raised by parameter correction
- Window area "manual movement" is cut up after zooming
Included Driver Function Blocks:
- CODESYS Point to point V3.5.10.44
- CODESYS SoftMotion V4.0.16.0
|
CMMT-ST_1.3.0.46.fsi
Deutsch [de], English [en]
File size: 49 MB
Version: 1.3.0.46 (28/11/2019)
|
|
Version 1.2.2.4 (02.10.2019)
Fixed Bugs:
- Calculated limits for current and torque too low for systems with spindle axes
Included Driver Function Blocks:
- CODESYS Point to point V3.5.10.40
- CODESYS SoftMotion V4.0.16.0
|
CMMT-ST_1.2.2.4.fsi
Deutsch [de], English [en]
File size: 48 MB
Version: 1.2.2.4 (02/10/2019)
|
|
Version 1.2.1.19 (21.08.2019)
New Features:
- Support for CMMT-ST-...-EP with Ethernet/IP interface (V1.2.1)
Fixed Bugs:
- Exception when entering certain feed constants
- Error when synchronizing string parameters with the device
- Text on button for releasing the holding brake not unreadable
- Reinit after changing the hardware switch settings not possible
- SoftMotion driver version not displayed
- User defined gear is deleted when changing the axis
- Zero point offset is not stored correctly in certain cases
- Reinit icons missing for some parameters
- Exception when editing an existing drive configuration
- Missing scroll bars on page Diagnosis -> I/O state
Included Driver Function Blocks:
- CODESYS Point to point V3.5.10.38
- CODESYS SoftMotion V4.0.16.0
Supported systems:
- servo drive CMMT-ST-C8-1C-EC-S0 (8084005)
- servo drive CMMT-ST-C8-1C-EP-S0 (8084006)
- servo drive CMMT-ST-C8-1C-PN-S0 (8084004)
|
CMMT-ST_1.2.1.19.fsi
Deutsch [de], English [en]
File size: 48 MB
Version: 1.2.1.19 (21/08/2019)
|
|
Version 1.2.0.25 (11.06.2019)
New Features:
- Support for CMMT-ST-...-PN with PROFINET interface
- Support for PositioningDrives data import
- Support for cam controller function (position trigger)
- Support for touch probe function
- Calculation of system limits:
- Warnings are shown if parameter values exceed calculated limits
- Dialog for resetting inconsistent parameters to recommended values
- First setup wizard:
- Supply voltage selection
- Consistency check for homing method and hardware switches
- Parameter pages:
- Order of contexts "Control" and "Diagnosis" changed
- Warnings on parameter pages are indicated in navigator
- Device details can be displayed on drive configuration page
- Consistency check for digital I/Os
- Simplified encoder settings
- Consistency check for homing method and hardware switches
- Software limits can be teached
- Trace improvements:
- Multiple signals can be selected when adding a trace channel
- Masking of individual bits for trace channels and trigger
- Possibility to share Y axis for signals
- Improved handling of several trace records
Fixed Bugs:
- Exception when entering certain feed constants
- Error when synchronizing string parameters with the device
- Text on button for releasing the holding not unreadable
- Reinit after chaning the hardware switch settings not possible
- SoftMotion driver version not displayed
- User defined gear is deleted when chaning the axis
- Zero point offset is not stored correctly in certain cases
- Reinit icons missing for some parameters
- Exception when editing an existing drive configuration
- Missing scroll bars on page Diagnosis -> I/O state
Included Driver Function Blocks:
- CODESYS Point to point V3.5.10.34
- CODESYS SoftMotion V4.0.14.0
Supported systems:
- servo drive CMMT-ST-C8-1C-EC-S0 (8084005)
- servo drive CMMT-ST-C8-1C-PN-S0 (8084004)
|
CMMT-ST_1.2.0.25.fsi
Deutsch [de], English [en]
File size: 48 MB
Version: 1.2.0.25 (11/06/2019)
|
|
Version 1.1.1.14 (03.04.2019)
New Features:
- Online help in German and English available
- Updated CODESYS function blocks
Supported Systems:
- Servo Drive CMMT-ST-C8-1C-EC-S0 (8084005)
|
CMMT-ST_1.1.1.14.fsi
Deutsch [de], English [en]
File size: 107 MB
Version: 1.1.1.14 (03/04/2019)
|
|
Version 1.1.0.109 (28.01.2019)
New Features:
Supported Systems:
- Servo Drive CMMT-ST-C8-1C-EC-S0 (8084005)
|
CMMT-ST_1.1.0.109.fsi
Deutsch [de], English [en]
File size: 57 MB
Version: 1.1.0.109 (28/01/2019)
|