Title:
Festo Automation Suite - Plug-in
Subtitle:
Plug-in for the parameterisation of CPX-AP automation systems
Document type:
Commissioning
Version Download
Version 1.5.0.215

New Features:

  • Connection is established faster (further improvement planned)
  • Forcing of process data of valve terminals
  • Additional information on diagnosis page "System State":
    • Display of cable length between modules
    • Display of module product keys
  • Support for VTSA adapters with slot for another module
  • Support for IO-Link connectors
  • Support for automatic creation of connections in topology editor


Fixed Bugs:

  • Deleting a CPX-AP-A module via the module list below the terminal view might cause inconsistent data
  • Application sporadically hangs when disconnecting from the device
  • Error log is not automatically read from the device when the "Error Log" page is opened while connected to the device
  • Parameters shown in German after saving and loading a project with a CPX-AP-A-EC interface module even though the language is set to English


Known Limitations:

  • For connecting to CPX-AP-I-4IOL-M12 modules, firmware V1.4.13 or higher is required
  • PROFIBUS interface modules are not supported since connecting to these devices is currently not possible
Version 1.4.1.7

Fixed Bugs:

  • Forcing of an output channel may unexpectedly change the state of another channel
  • Moving, replacing or deleting modules in a terminal may lead to corrupt project data
  • CPX-AP-A-12DI4DO-M8-4P module not displayed correctly


Known Limitations:

  • Connecting to larger system takes a while
  • Forcing of process data is not yet supported for valve terminals
  • For connecting to CPX-AP-I-4IOL-M12 modules, firmware V1.4.13 or higher is required
  • PROFIBUS interface modules are not supported since connecting to these devices is currently not possible
Version 1.4.0.315

New Features:

  • Support for CPX-AP-A terminals:
    • Terminal view for adding, removing and replacing modules within a terminal
    • Catalog in the right sidebar with available modules
    • Navigation to parameter pages of the configured modules in the left sidebar
    • Display of the terminal configuration in topology editor
  • Online mode:
    • Display and forcing of process data
    • Diagnosis page "System State", providing a list of all connected AP devices incl. voltages, cable lengths and diagnosis information (only available in the plug-in instance of the interface module or the terminal that contains the interface module)
    • Improved performance if a connection attempt to the system fails or is cancelled
  • When connected to a PLC in topology editor:
    • CODESYS devices for modules are named according to the module description or name


Fixed Bugs:

  • Connection attempt to CPX-AP-I-PN fails
  • Renaming of devices is not properly taken into account under certain circumstances when exporting Rockwell L5X


Known Limitations:

  • Connecting to larger system takes a while
  • For connecting to CPX-AP-I-4IOL-M12 modules, firmware V1.4.13 or higher is required
  • PROFIBUS interface modules are not supported since connecting to these devices is currently not possible
Version 1.3.1.6

Fixed Bugs:

  • Diagnosis page "Parameters" is not displayed
  • Modules appear online after the connection to the system is lost
  • CPX-AP-I-4IOL variant setting is not applied to CODESYS
  • Connection attempt to CPX-AP-I-EP sporadically fails
  • Rockwell L5X export sporadically fails


Known Limitations:

  • Process data are not yet available
  • For connecting to CPX-AP-I-4IOL-M12 modules, firmware V1.4.13 or higher is required
Version 1.3.0.198

New Features:

  • Online mode:
    • Establishing a connection to CPX-AP-I-EC, -EP and -PN possible (for -EC via Ethernet over EtherCAT or the "TP2" port while disconnected from the PLC)
    • Parameter values are compared when establishing the connection and can be written to or read from the system
    • Parameter values are cyclically updated while connected
    • Parameter changes applied immediately when connected to the device
    • Display of current diagnostic messages per module
    • Display of the error log of the interface module
    • Display of the device state in topology editor
  • When connected to a PLC in topology editor:
    • CODESYS device editor available on parameter page "CODESYS"
    • Selection of the CODESYS device version possible
  • Device details shown in right sidebar

Fixed Bugs:

  • EtherCAT startup parameters are not generated properly when connected to a PLC in topology editor
  • Status of the CODESYS device is not shown when connected to a PLC in topology editor


Known Limitations:

  • Process data are not yet available
  • For connecting to CPX-AP-I-4IOL-M12 modules, firmware V1.4.13 or higher is required
Version 1.1.1.7

Fixed Bugs:

  • Rockwell L5X export:
    • Syntax error in export file
    • Status assembly too big when using more than 40 modules
    • Consistency error when using VAEM pneumatic adapters
  • CPX-AP-I-EC configuration error when deleting and restoring the connection to the EtherCAT system in topology editor


Known Limitations:

  • Only systems with CPX-AP-I-EP and -EC interface modules are supported.
  • Connecting to the device is not possible yet.
  • Diagnostic messages and process data are thus not yet available.
Version 1.1.0.99

New Features:

  • Rockwell parameter export for large systems (using Large Forward Open)
  • Support for configuring AP systems connected to Festo controllers in topology editor:
    • Support for CPX-AP-I-EC EtherCAT interface module
    • CODESYS package automatically installed along with the plug-in (no need to install EtherCAT ESI file manually)
    • CODESYS devices for AP modules automatically synchronized with the AP system configuration
    • Parameterization of modules via the plug-in's user interface
    • Automatic transfer of parameters into the EtherCAT startup parameterization data
  • Darker device images for improving the contrast in topology editor


Fixed Bugs:

  • Error in Rockwell export if IOL module is mounted behind other output module
  • Unsupported parameters shown for valve terminals


Known Limitations:

  • Only systems with CPX-AP-I-EP and -EC interface modules are supported.
  • Connecting to the device is not possible yet.
  • Diagnostic messages and process data are thus not yet available.
Version 1.0.0.333 (12.02.2021)

First Release

Features:

  • Export of the system configuration and parameters for Rockwell Studio 5000


Known Limitations:

  • Only systems with CPX-AP-I-EP bus interface are supported.
  • Connecting to the device is not possible yet.
  • Diagnostic messages and process data are thus not yet available.