Title:
Firmware Package
Description:
Supported systems:
  • servo drive CMMT-AS-...-11A-P3-... (5111189)
  • servo drive CMMT-AS-...-3A-... (5111184)
  • servo drive CMMT-AS-C12-11A-P3-MP-S1 (8143169)
  • servo drive CMMT-AS-C18-11A-P3-MP-S1 (8157801)
  • servo drive CMMT-AS-C2-11A-P3-MP-S1 (8143165)
  • servo drive CMMT-AS-C2-3A-MP-S1 (8143163)
  • servo drive CMMT-AS-C25-11A-P3-MP-S1 (8157802)
  • servo drive CMMT-AS-C3-11A-P3-MP-S1 (8143166)
  • servo drive CMMT-AS-C4-3A-MP-S1 (8143164)
  • servo drive CMMT-AS-C5-11A-P3-MP-S1 (8143167)
  • servo drive CMMT-AS-C7-11A-P3-MP-S1 (8143168)
  • Software FESTO AUTOMATION SUITE (8074657)
Document type:
Firmware
Version Download
Version V352 (02.09.2024)

New Feature:

  • Firmware package files have been renamed, and the versioning format has been changed:
    CMMT-MP-V34.0.13.18_Release.pck -> drive-hp-g1_35.9.1.pck
  • Position-dependent torque control:
    It is now possible to specify a torque as a feedforward value for the control based on the position. More information can be found in the documentation.
  • Modbus timeout can be set via FAS using parameter Px.102393.
  • Support for multiple parameter sets:
    The device supports up to 4 different parameter sets, each stored in a slot. The web server can be used to set which parameter set should be active on the next restart. This allows for quick switching between different configurations.
  • Extended parameterization options for Hiperface encoders:
    - Enable manual parameterization using Px.64140
    - Enter the number of Sin/Cos cycles per revolution from product information in Px.6412
    - Enter the number of singleturn resolutions per revolution in Px.6413
    - Enter the multiturn resolution per revolution in Px.6414
    - Select whether multiturn encoder is used in Px.6415
    - Select whether linear encoder is used in Px.100000

Fixed Bugs:

  • Direction reversal in master-slave operation is not detected.
    Changes to the direction reversal Px.1170 affect the configuration of X10.
  • Gear In/Out as a slave via X10 interface can cause a software crash (status led is flickering red).
  • Modbus connection is not properly closed by disconnecting and reconnecting the cable.
    Reconnection is now performed correctly.
  • Drive can be released by fieldbus when control authority is set to "I/O".
    It is not possible to release the drive via fieldbus when control authority is set to "I/O".
  • Digital output linkage "Bit 16 CiA402 0x60FE" and "Bit 17 CiA402 0x60FE" is not selectable for CMMT-ST.
  • CiA object 0x60FE (digital outputs) is not updated.
    Parameter P1.1128054 (mapped to CiA402 object 0x60FE) is not updated when changing outputs through the motion profile or fieldbus.
  • Holding brake cannot be opened via FAS while STO is active.
  • Current position in module operation in the module window area remains 0.
  • Referencing with EMMB-AS can be lost on device restart.
  • Unexpected error message "Process data connection lost" in combination with EtherNet/IP and Modbus.
    This was reported although no control is requested via control word 1 (STW1) bit 10.
  • An input offset can be used for the analog input before the deadzone using parameter Px.102673.
  • Improved evaluation of stroke limits for referencing methods with automatic direction reversal.
    For all referencing methods where the search direction is reversed, for example, when reaching a stop, it is now possible to adjust the stroke limit monitoring independently of the direction.
  • Warning "Incorrect IP address settings" after changing the telegram selection with EtherNet/IP.
    The IP address remains unchanged.
  • With CMMT-ST-MP in combination with a motor with a holding brake, the brake is not opened by a configured digital input.
    The holding brake is opened by setting the configured input.
  • PROFIdrive telegram 103 and telegram 4 cannot be used with IRT / AC4.
    Both telegrams can also be used with IRT / AC4.
  • For manually configured Hiperface encoders, when the parameter Px.6412 does not correspond to a power of 2, the target position is calculated incorrectly.
    The configuration of arbitrary values in the parameter Px.6412 is supported.
Version 34.0.13.18 (02.04.2024)

New Feature:

  • Modulo with tolerance window
    To ensure the same number of turns or movement is obtained in case of small position differences after turning on the device with multiturn position encoders or after a reference run, it is possible to configure a tolerance window using Px.102100. Within the tolerance window, movements against the commanded direction may occur. The behavior compatible with firmware V33 can be activated with parameter Px.102137.
  • CiA402 Save extension Motor rated current (conformity)
    The value written via the object 0x6075 motor_rated_current is saved in the parameter Px.7118. If the value written is greater than the rated current stored in parameter Px.7117, the value written is limited to the value in parameter Px.7117. If parameter Px.7118 contains a lower value than parameter Px.7117, the lower value is retained, even if a motor with a higher rated current is subsequently configured with the current plug-in. If the message for the parameter Px.7118 Project=1e37Arms and Device=0.10Arms appears in the adjustment window with the current plug-in, the high value must be written to the device. The CMMT then limits to the correct nominal current as described above.
  • Modulo for relative motion command
    The Modulo operating mode has been extended for the relative motion command. A more detailed description is provided in the documentation.
  • Enhanced torque control
    An analog input can be used to connect and evaluate a torque/force sensor for the CMMT-AS device family. This allows for improved torque control on the output without the influence of friction. A more detailed description is provided in the documentation.
  • Jog operation with configurable delay
    Enhanced parameterization option for jog operation. You can choose whether to use a symmetric (default, old behavior) or asymmetric brake ramp for jog operation. The following parameters can be set via the expert list for symmetric jog operation:
    - Selection of symmetric or asymmetric jogging (Px.102395)
    - Desired brake ramp 1 for slow movement of jog operation (Px.102397)
    - Desired brake ramp 1 for fast movement of jog operation (Px.102401)
    - Desired brake ramp 2 for slow movement of jog operation (Px.102407)
    - Desired brake ramp 2 for fast movement of jog operation (Px.102413)
  • Enable Servo Drive, Activation via "I/O or fieldbus"
    The parameter (Px.10232) for the device has been extended with the option for enable servo drive via "I/O or Fieldbus".
  • Master-Slave without down synchronization
    For Master-Slave operation, it is possible to specify "without down synchronization" for the Gear-Out method. When this option is used, the slave drive remains permanently synchronized with the master without considering the Gear-Out limits. As long as no new motion command is sent to the slave drive, it remains synchronized with the master.

Fixed Bugs:

  • Factory reset does not reset fieldbus configuration to PROFINET.
    After activating the factory reset, the previous fieldbus configuration remains unchanged.
  • EtherCAT timeout during file transfer (FoE)
    A timeout during file transfer (FoE) no longer occurs.
  • Modbus TCP "Communication timeout" register is not stored non-volatile.
    The configuration is stored non-volatile in parameter Px.102393 (default 1s).
  • Software limit error
    The detection of a violation of the software end position with error reaction is recognized upon first entry. Further error reactions are suppressed, for example, when a vertical axis sags and returns to the power-on position. Triggering an error reaction is only activated again when the set position is within a valid position range.
  • Direction lock in controlled operation
    The direction lock is taken into account in controlled operation.
  • Faulty behavior of the trajectory generator during sequence change in record table with touch probe.
    Optimized trajectory generator regarding touch probe.
  • Drive cannot be enabled near the software end position.
    The behavior for enabling the drive near the software end position has been improved, allowing the drive to be enabled.
  • Synchronization error when operating with an IRT switch.
    The synchronization error no longer occurs.
  • Cia402: Fault reaction interrupted by control word.
    Changing the control word during "Fault" or "Fault Reaction" status has no impact.
  • No Modbus connection possible after unplugging and reconnecting the cable.
    Modbus connection can be restored.
  • Possible position jump in conjunction with multiturn encoders.
    Referencing is reset in case of an invalid extended multiturn position.
  • Faulty diagnosis "Motor change detection" reported during encoder interruption.
    The faulty diagnosis is no longer reported.
  • Invalid gear ratio during field weakening.
    Correct gear settings are used.
  • Modbus timeout not adjustable via plugin.
    The Modbus timeout can be adjusted via the plugin.
  • Fieldbus selection reset to PROFINET by updating the firmware to version 34.0.11.
    The fieldbus selection is no longer changed by the firmware update.
  • ABI encoder signal too weak for long cable lengths.
    The default threshold has been changed.
  • Unintended occurrence of 'Calculation of mass/friction value estimate not completed' warning.
    Unintended warning prevented.
  • Internal motion monitoring P1.460 Bit 0 (TRX) not only dependent on monitoring window target position.
    Internal motion monitoring TRX is set via monitoring window target position and damping time.
  • CMMT-ST-MP: Digital output, it is not possible to link it to CiA402 0x60FE / Bit 16 and 17.
    The setting options have been expanded.
  • EMMB-AS: The referencing will be reset
    The referencing will be retained after a successful referencing even after a device restart.
Version 33.0.10.12 (05.10.2023)

Version changes:
Fixed Bugs:

  • IP configuration is lost with EtherNet/IP
  • Dynamic increase of the torque limit
  • Loss of the referencing status
Version 33.0.9.10 (30.06.2023)

Firmware Package

Version 32.0.9.9 (19.01.2023)

Firmware Package

Version V031.0.9.13 (20.10.2022)

Firmware Package

Version V031.0.8.12 (05.10.2022)

Firmware Package

Version V031.0.7.10 (04.07.2022)

Firmware Package

Version V030.0.6.6 (28.04.2022)

Version changes:
CMMT-AS-MP Firmware only PROFINET