White paper: Plants based on the Lego principleModular automation with valve terminals
White paper: Plants based on the Lego principle
Special publication

Smaller batches and different types of product in the same plant – these are the market demands to which more and more manufacturers in

the process industries need to adjust. The answer is plants based on the “Lego principle”. Users can add modules or switch them off in line

with requirements. But this is only possible with modular automation.