Title:
FluidDraw P6 Full version
Subtitle:
License required! You get it via the Festo App World.
Document type:
Software
Version Download
FluidDraw setup 6.2p

1. An error message may have appeared when changing the cable designation.
2. The interface to online shopping carts is now working again after a major technology change.
3. For some base length units, the position of the piston rod of the configurable cylinders was not calculated correctly.
4. In rare cases, the reports could move unintentionally.
5. The description of components in the properties dialog was sometimes not applied immediately.
6. Some valve designations were not assigned correctly during order code resolutions.
7. In rare cases, a misleading message appeared when saving to network drives.
8. Changes to common properties of multiple selected lines were sometimes not applied correctly.
9. The defined pen properties can now also be applied to cable symbols and terminals.

FluidDraw setup 6.2o

1. Fixes an error when sending large parts lists to the Festo online shop.
2. Fixes an error when importing product databases.
3. Improves the symbol search in the component library.
4. The common line properties were sometimes not transferred correctly.
5. When inserting symbols, text blocks were sometimes outside the drawing area.
6. The “Object appears in parts list” property was not always handled correctly when deleting secondary objects.
7. Improves the scaling and rotation of macro objects via the properties dialog.
8. Fixes an error when enlarging dialog windows.
9. Text objects can now be assigned a background color.
10. The list of drawing layers now always displays their names.
11. FluidDraw now responds immediately after closing the options dialog. Previously, there was a short pause during which the program was unresponsive.
12. Fixes a bug when editing text IDs within user attributes.
13. Activating a sheet in the project tree would, in rare cases, open a sheet with the same name from another project that was currently open.
14. When duplicating projects, references to global objects were sometimes not set correctly.
15. FluidDraw could behave incorrectly if the Windows directory for temporary files contained too many files. This is now handled correctly and a message is displayed if necessary.
16. During installation, the version of the CodeMeter license driver that may already be installed is determined more reliably.
17. The supplied excerpt from the Festo product catalog and the symbol library have been updated.
18. The link between contacts and relay coils could be lost in rare cases.
19. When adding a new sheet via the project tree, the sheet appears under the active node.
20. The entered folder paths are now taken into account correctly again.
21. When inserting some modular products, the symbol was not assembled correctly.
22. Inserted product photos from the product catalog no longer receive a symbol name.
23. The background color of evaluations is now handled correctly.
24. Improves the arrangement of symbol attribute texts.
25. Improves the automatic numbering of valve island labels.
26. Increases program security through various measures and checks.
27. Fixes a rare error during update installation.
28. The “Reverse direction” option now also works for electrical lines in the common properties dialog.
29. Fixes the error that sometimes unresolved attribute texts are generated.
30. For some base length units, the position of the piston rod of the configurable cylinders was not calculated correctly.
31. Improves the alignment of text within cross-references.

FluidDraw setup 6.2n

1. The web addresses of the online services have been updated.
2. Updates the supplied Festo product catalog extract and the symbol library.
3. Improves the display of the cumulative parts list.
4. Improves the insertion of parts lists from Festo QuickSearch.
5. The CSV export of parts lists is now done by default without quotation marks.
6. Fixes an error when pasting rotated objects from the clipboard.
7. Fixes a rare error when opening the project properties via the context menu in the project tree.
8. Improves the transfer of a parts list to the Festo shopping cart.
9. In rare cases, the contact images were not displayed correctly.
10. Inserting cross-references sometimes did not work.
11. Contains various optimizations for editing large projects.
12. If an object is deleted that is referenced by text references, a prompt asks whether the references should also be deleted.
13. The context menu of a text reference now includes a new option for deleting the object referenced by the text.
14. Text objects can now be assigned a background color in addition to a foreground color.
15. If the main object to which secondary symbols refer is deleted, the option for the object to appear in parts lists is now kept.
16. When a macro-object is scaled, the scaling factors in the properties dialog are now displayed correctly.

FluidDraw setup 6.2m

1. The representation of T-distributors has been adapted to the current standard.
2. Connected components were sometimes not handled correctly when distributing a valve terminal.
3. Sometimes no global object was created when inserting a valve terminal.
4. Improves the zoom function with the mouse wheel while holding down the Ctrl key.
5. The catalog dialog now remembers the last database used.
6. Fixes a bug when scaling multiple selected texts.
7. Corrects the dialog of the geometry properties of simple lines.
8. User-defined attributes were sometimes lost when changing the properties of several selected lines.
9. Updates the supplied Festo product catalog extract and the symbol library.

10. The automatic line designation did not work.

FluidDraw setup 6.2l

1. Fixes a display error when searching for attribute links.
2. The cursor position is taken into account when inserting attribute links.
3. Fixes an error when automatically connecting components.
4. Prevents duplication of prefixes in designations.
5. Designations of T-distributors are now numbered correctly.
6. The creation of components containing certain special characters now succeeds.
7. Fixes a bug in the designation of sub-objects.
8. Improves the insertion of parts lists from QuickSearch.
9. The actual components are now highlighted more clearly when renumbering.
10. Improves the position of line attributes.
11. Updates the supplied Festo product catalog extract and the symbol library.
12. The option "invisible objects appear in parts list" is now correctly interpreted in the reports.
13. Prevents the program from freezing in case of cyclic references.

FluidDraw setup 6.2k

1. Updates the supplied Festo product catalog extract and the symbol library.
2. Labelling rules were not saved correctly with the project/page node.
3. The defined font was not always used for the designation of connection lines.
4. Corrects an error in the designation numbering.
5. Improves the positioning of inserted symbols.
6. Improves the display and text alignment of line attributes.
7. The preview images of unplaced objects were sometimes not displayed correctly.
8. When renumbering designations, the active component was sometimes not highlighted.
9. Corrects a line dragging error.
10. Corrects an assignment error in user databases with part numbers that collide with Festo products.
11. Sometimes wrong symbols from user libraries were used when creating circuits from an order code.
12. Shortened representation of label connections was sometimes lost after saving.
13. Inserting cross-references sometimes did not work correctly.
14. Encrypted files sometimes could not be printed.
15. Fixes an error when automatically translating the component description.
16. Attribute links were not always set correctly when copying object groups.
17. Attribute links to lines are now displayed correctly.
18. Improves automatic naming of symbols when inserting them into user libraries.
19. Improves calculation of column width in reports.
20. If an error occurs when inserting an order code, a more meaningful message now appears.

FluidDraw setup 6.2j

1. Fixes an error that occurred when merging columns in reports.
2. Corrects the location of cables in reports.
3. Improves Internet access to Festo online services.
4. Corrects incorrect attribute links and object references when copying symbols (global objects) to another project.
5. Corrects a layout error in the about box.
6. Displays a message when incorrect values are entered in the options dialog.
7. Extends reports by the columns installation/location/circuit of components.
8. Updates the supplied Festo product catalog extract and the symbol library.
9. Corrects an error in connection with Internet access under Windows 7.
10. Fixes an error when distributing valve terminals to several pages.

FluidDraw setup 6.2i

1. When copying pages, the global objects are optionally copied as well.
2. More detailed messages appear if errors occur when inserting valve terminals.
3. Texts can now be anchored to reports.
4. If valve terminals are distributed to several pages, the positions of the identifiers are kept.
5. Changed identification letters now also affect user libraries.
6. Symbols from QuickSearch are inserted into the existing FluidDraw instance even if the option "Allow multiple FluidDraw instances to be started" is enabled.
7. Improves the full text search in the component library.
8. With an update installation, the help files are installed correctly.
9. Improves the display of attribute texts when inserting valve terminals.
10. Sub-objects are correctly incremented when copying.
11. In the common properties the designations of the connections can be shown or hidden.
12. The setting of connection terminators for multiple selected connections has been improved.
13. Updates the supplied Festo product catalog extract and the symbol library.

FluidDraw setup 6.2h

1. The “Go to Target” function sometimes did not jump to the correct object.
2. Improves the full text search in the component library.
3. The current circuit generation is now used for manual order code entry under “Insert from catalog”.
4. Line breaks within cross references were not always handled correctly.
5. Libraries that were included as symbol folders were not always opened read-only.
6. The installer now supports a parameter to control the automatic check for updates for all users.
7. Speeds up the search for licenses on the network.
8. Updates the supplied Festo product catalog extract and the symbol library.

FluidDraw setup 6.2g

1. Cross references to non-unique reference designations are preserved.
2. Attribute links were not resolved correctly if the project path contains the meta character for “multiple attributes in one line”.
3. Page names composed of translations in the project tree are displayed better.
4. The designations of multiple sub-objects was not always incremented correctly.
5. Sometimes the correct catalog symbol was not inserted when overwriting predefined symbol kits with custom libraries.
6. When inserting via QuickSearch or from a file, the option for inserting “legacy valve terminal symbols” was not correctly taken into account.
7. When exporting single pages of a project, cross-references were sometimes not displayed correctly.
8. Editing attribute values in reports now works even if attribute names contain blanks.
9. File and web links are now available in the column selection for reports.
10. Improves the position of connector texts for some symbols.

FluidDraw setup 6.2f

1. Images from the clipboard could be inserted erroneously in the editing dialog of the text objects.
2. When editing reports interactively, pasting from the clipboard was sometimes misinterpreted.
3. Transferring the catalog properties of multiple selected connectors now works correctly.
4. The symbols of silencers and blind plugs have been revised.
5. Ident codes containing spaces are now resolved correctly.
6. Corrects some menu translations.
7. Sub-symbols now keep their own symbol names.
8. Some attribute links were not updated when inserting objects from custom databases.
9. Fixes a rare error when arranging valve terminals.
10. Pages containing reports were not always correctly fitted via “Fit to window”.
11. If components are inserted without a symbol, the type attribute is now displayed correctly.
12. The menu item “Insert relates symbol” is now also available for grouped single objects.
13. Updates the supplied Festo product catalog extract and the symbol library.
14. Improves SVG export and graphical representation in the clipboard.
15. Corrects internal rounding errors on loading circuit files.

FluidDraw setup 6.2e

1. When interactively moving pages in the project tree, page nodes could accidentally disappear.
2. The dialog for DXF import sometimes did not show a preview.
3. Sometimes designations inside macros were displayed erroneously.
4. Predefined attributes of user databases were not always handled correctly.
5. "Order code 1", "Order code 2" and "Description" are now available for user databases both in the import dialog and when manually assigning user attributes.
6. The CodeMeter driver installation sometimes failed on Windows Server systems.
7. In the options dialog there are several settings for the text output in the DXF export.
8. Inserting valve terminals failed when the reduced view was set in the component library.

FluidDraw setup 6.2d

1. When printing and exporting, pages in the parts list view were sometimes not displayed correctly.
2. When exporting, the selection of pages is retained until the next program start.
3. The dialog for the cable properties was sometimes not displayed correctly.
4. In rare cases, pages could not be moved in the project tree.
5. Improved error handling when resolving ident codes for valve terminals.
6. Fixed an error when renumbering identifiers when multiple projects are open.
7. Line ends in properties dialogs are now more distinguishable.
8. The language settings in the options dialog are now grouped on one page.
9. A message appears that the interface to the new Festo online shopping cart is not yet functioning.
10. Attribute links with properties of main objects now bring a reduced dialog.
11. Snap options now affect the already drawn line segments of the polyline being created.
12. In the project window the active project is highlighted more clearly.

FluidDraw setup 6.2c

1. The management of user libraries contains various plausibility checks.
2. The position of the reference identification has been improved.
3. Fixes an error related to translations within the reports.
4. The call of online services has been updated.
5. Line style of lines on layer level is now correctly handled for PDF export.
6. Assigned keyboard shortcuts are displayed in the configuration dialog for the menu ribbons.
7. The active page is highlighted more clearly in the project tree.
8. Moving folders and pages in the project tree is now better visualized.
9. When a project tab is activated in the project window, the last active page of the associated project comes to the foreground.
10. The cursor keys can now be used to navigate through the project tree as follows:
- ENTER –> Open selected page. If the SHIFT key is pressed, the current page is closed, if it belongs to the same project.
- SHIFT + UP/DOWN –> Open next page. The current page will be closed if it belongs to the same project.
- DEL –> The selected page or project node is deleted after confirmation.
- The following was already possible: CTRL + UP/DOWN –> Moves the selected node in the project tree.
11. Fixes an error that could lead to the loss of object references.
12. If a group was deselected, sometimes connectors within the group remained selected.
13. Line end symbols were sometimes swapped when drawing lines.
14. An option allows FluidDraw to be run multiple times.
15. In the context menu of the library window there are now special commands for updating, freeing and editing user libraries that are open at the same time.
16. A suitable preselection is displayed in the quick filter of the reports.
17. In template management, copies of existing templates are better named.
18. The dialog for designation rules now checks the validity of user entries.
19. Improves line routing for connectors that are not exactly on the grid.
20. When creating multiple connection lines, existing source connections are now better taken into account.
21. Updates the supplied Festo product catalog extract and the symbol library.
22. Optimizes loading of large projects with many embedded images.
23. Improves the quality of vector graphics when copying circuits to the clipboard.
24. Loading, printing and exporting of large projects is mostly done in the background and can be aborted before the end.
25. FluidDraw now uses Festo’s online service for symbol generation from order codes. This requires an Internet connection.
26. Fixes a rare crash with reference loops.
27. The setup contains the CodeMeter Runtime 7.40.

FluidDraw setup 6.2b

1. In the dialog for selecting the automatically displayed attributes, several attributes with the same name are grouped together and listed only once.
2. The retrieval of the online service for spare parts search has been updated.
3. The numbering sequence of the valve solenoid designations has been revised.
4. Fixes a rare error when editing product databases and translation tables.
5. The “Inherit from page” option was not saved correctly for the “Circuit” property of an object.
6. Cable symbols without assigned wires could cause an error in the object browser.
7. The display and interactive editing of reports has been improved.
8. Supports multiline display of cell contents in reports.
9. Support for text IDs and attribute links in static tables Improved.
10. Symbols and minor function updates are now done via the online update without having to update the complete program.
11. When exporting reports, the columns to be exported can now be selected.
12. In the context menu of a symbol all linked symbols are now listed as jump targets.
13. Texts, text IDs from translation tables and attribute links can now be written in one line in the text object, provided they are separated from each other by a definable delimiter symbol. For compatibility reasons, this feature is disabled by default and can be enabled in the project properties.
14. The user name is available as a predefined variable (%UserName).
15. If a text ID from the translation table is inserted into a text object while the “attribute link” option is activated, it is automatically enclosed in quotation marks.
16. When an attribute link is inserted, it is automatically shortened if the referenced object is on the same page as the text object.
17. The project tree in the browse dialog for attribute links now highlights the selected link or the last selected node, depending on the context.

FluidDraw setup 6.2a

1. Editing the parts list cells did not work anymore in version 6.2.

2. Fixes a crash when opening the font dialog box multiple times since version 6.2.
3. Textual search improved in the component library.
4. The behavior of text links for components without symbol has been improved.
5. Adds various symbol generations for component symbols.
6. Suppresses the generation of unwanted labels when pasting symbols from the clipboard.
7. Prevents the creation of a global object when inserting a macro from the user library.
8. Fixes a designation error when editing multiple potentials or interruptions at the same time.
9. User-defined templates can now be deleted in template management.
10. In the ribbon bar there are now commands to show and hide the component library, the project tree and the object browser window.
11. The file size for PDF export is now significantly reduced.
12. The license server is now found more reliably after a network interruptions.
13. Automatic line routing at T-distributors have been improved.
14. Fixes a preview error for configurable valves and cylinders.
15. The setup installs the CodeMeter Runtime 7.21a, which contains security improvements.