Title:
Error 4000 with CMMB-AS and EMMB-AS
Subtitle:
EMMB-AS
Description:

When connecting the new generation of EMMB-AS on an CMMB-AS the driver shows error 400.0 in the display which cannot be acknowledged

Document type:
Application Note
Title Version

Application Note - Error 4000 with CMMB-AS and EMMB-AS

 

When connecting the new generation of EMMB-AS on an CMMB-AS the driver shows error 400.0 in the display which cannot be acknowledged