Title:
Firmware
Subtitle:
Firmware CPX-AP-I-4IOL-M12
Description:

Supported systems:

  • IO-Link Master CPX-AP-I-4IOL-M12 (8086604)
  • Remote I/O system CPX-AP-I (8094920)
Document type:
Firmware
Version Download
Version 1.6.12

Features:

  • delay start of IO-Link communication after power-on
Version 1.6.10

Features:

  • Add parameter for virtual AP address

 

Fixes:

  • PL diagnosis raise/resolve on startup
  • Improve AP transmission quality
Version 1.6.6

Features:

  • Change cycle time calculation, use best-case when possible.
  • Start IO-Link communication earlier after power-on.
  • More statistics in case of AP communication errors and change the counters to wrap.

Fixes:

  • Port diagnosis when Device I/O is larger then PLC configured size. Only when supported by the AP Fieldbus Interface.
  • Sporadic incorrect wirebreak detected diagnosis (#5402018).
  • In some situations reset to factory does not reset all settings (#539998, #6093303).
  • Support parallel ISDU requests (#5138362).
  • Fix sporadic IO-Link diagnosis messages in case of power supply lost (#5692723).
  • Fix communication cycle time for devices with more than 8 PD output bytes (#5892735).
Firmware
Version 1.5.6

Features:

  • AP connector types in description
  • Add error when the IO-Link master port stops updating

Fixes:

  • Frozen IO-Link master port after 5 days in case of IO-Link Device cycletime error(s)
  • LED behaviour on AP Identify command
  • MD LED behaviour on AP bus restart
Version 1.4.13

Features:

  • The port configuration is applied on any change (not only on change of port mode).
  • The port configuaration is stored stored in non-volatile memroy. If port mode is set to IO-Link the IO-Link connection will be established directly after power on.

Fixes:

  • The IO-Link connection is restarted 500 ms after a device lost instead of directly after.
  • Cleared datastorage content is encoded as 12 zero bytes (all header entries 0) instead of 0 length data in SMI.