Title:
CMMT servo drive commissioning MITSUBISHI IQ-R PLC by ETH/IP
Subtitle:
CMMT-AS; Mitsubisi IQ-R PLC with ETH/IP; Library included
Description:

This Application Note gives detailed procedure to integrate CMMT

Servo Drive with Mitsubishi IQ-R Controller in EtherNet/IP communication
network. Also described to Read/Write the servo motor parameter.

Document type:
Application Note
Title Version
CMMT servo drive commissioning with MITSUBISHI IQ-R PLC by ETH/IP

This Application Note gives detailed procedure to integrate CMMT

Servo Drive with Mitsubishi IQ-R Controller in EtherNet/IP communication
network. Also described to Read/Write the servo motor parameter.

使用 MITSUBISHI IQ-R PLC 通过 Ethernet/IP 调试 CMMT 伺服驱动器

本应用说明详述了在 EtherNet/IP 通信网络中将 CMMT 伺服驱 动器与 Mitsubishi IQ-R 控制器集成所需的过程。同时介绍了如 何在不同工作模式下控制伺服电机以及读/写伺服电机参数。