|
|
Version 19.0.6.16
New functions:
Fixed bugs:
- Bugfix: The incompatibility problems with some IO-Link masters due to a newer HW revision of the IO-Link chip have been fixed by an automatic trimming via the FW (Note: After a "downgrade" to an older FW version, the incompatibility problems may occur again).
Others:
|
Festo-EMCS_ST_V019.0.6.16_release-20221220-IOLFW1.0.iolfw
File size: 848 KB
Version: V19.0.6.16 (20/12/2022)
|
|
|
Version 19.0.5.7
New functions:
Fixed bugs:
- IO-Link data storage handling and establishment of communication were improved in relation to the usage of some affected masters
- The IO-Link events (warning) "Application warning - Start Press position out of range" and "Application warning - End position out of range" can both be quitted by the corresponding command performed in any known ways (process data bit, system command, digital inputs, Edit button of the HMI)
Others:
|
Festo-EMCS_ST_V019.0.5.7_release-20220318-IOLFW1.0.iolfw
File size: 848 KB
Version: V19.0.5.7 (18/03/2022)
|
|
|
Version 19.0.4.107
New functions:
- Firmware-Update / parameter set transfer functionality added (IO-Link)
- "Intermediate position" functionality added (only IO-Link: cyclic and acyclic device data, SystemCommands)
- "Auto Store Active" mechanism for activating/deactivating automatic saving of parameters in flash memory added (IO-Link). Plus additional display of the number of performed storage operations "Storage parameters".
Solves problem that frequent changes to individual parameters can lead to a device defect.
- Quit Error by DI-combination 1-1 added (identical for DIO & IO-Link).
Solves problem that error in DIO-mode can only be quitted by logic power cycle.
- Variable "Error Code" added (shows eventcode on HMI in a readable version also in IO-Link)
- New events added for error in intermediate circuit, during parameter set transfer and during FW-update.
- Addition of DataStorage parameter list by parameters for intermediate position and IO-Link tags (Application specific Tag, Function Tag, Location Tag)
- Two new system commands added for executing reference movement with end position detection.
Combines the reference movement with end position detection, which had to be executed by 2 separate parameters up to now, in one system command.
- Behaviour of actuator changed: Current movement is stopped, when HMI (Pushbuttons) are pressed and HMI-menu is opened.
Fixed bugs:
- Change of behaviour when entering value "0" for the 3 position parameters.
- Minor bugfixes.
Others:
- Behaviour in IO-Link mode changed: Values for position "Start Press" and "Intermediate Position" are overwritten with the new value of parameter "End Position Out" and reduced to this value, if their values are higher than the new value of "End Position Out".
- Added dynamic adaption of correction velocity. Applies only in case of tracking error.
- Change / dynamic adoption of structure of internal data model.
- Renewal of IO-Link-Stack regarding data transfer function and integration of improvements.
- Continuous Integration: Continuous adaption to further development of Festo automation platform.
- Minor improvements in code.
|
Festo-EMCS_ST_V019.0.4.107_release-20210315-IOLFW1.0.iolfw
File size: 847 KB
Version: V19.0.4.107 (15/03/2021)
|
|
|
Version 16.0.18.92
New functions:
Fixed bugs:
Others:
- Refactoring: General revision / review of code for higher stability and better comparability of firmware inside Festo automation platform.
- Change of internal IO-Link integration.
- Addition / Improvement in internal debug option.
- Minor improvements in code.
|
Festo-EMCS_ST_V016.0.18.92_release-20210209-IOLFW1.0.iolfw
File size: 865 KB
Version: V16.0.18.92 (20/07/2020)
|
|
|
Version 16.0.17.87
New functions:
Fixed bugs:
- Error after restoring factory settings fixed.
- Minor changes in bootloader (LED-sequence on HMI during startup).
- Minor bugfixes.
Others:
- IO-Link events are no longer permanently stored in memory.
- Continuous Integration: Continuous adaption to further development of Festo automation platform.
- Minor improvements in code.
|
Festo-EMCS_ST_V016.0.17.87_release-20210209-IOLFW1.0.iolfw
File size: 963 KB
Version: V16.0.17.87 (16/12/2019)
|
|
|
|
Festo-EMCS_ST_V016.0.15.72_release-20210209-IOLFW1.0.iolfw
File size: 955 KB
Version: V16.0.15.72 (23/08/2019)
|