Title:
Replacement of SDE1 Sensors by SPAU on MS
Subtitle:
Replacement of SDE1 Sensors by SPAU on MS
Description:

When using an MS module with integrated SDE1 Sensor (in MS type code, exemplarily MS4-LRB-1/4-D5-AD3-OS-AS - the sensor is indicated with AD1 to AD4)

Document type:
Application Note
Title Version
Replacement of SDE1 Sensors by SPAU on MS

When using an MS module with integrated SDE1 Sensor (in MS type code, exemplarily MS4-LRB-1/4-D5-AD3-OS-AS - the sensor is indicated with AD1 to AD4