Title:
Firmware (VBL)
Subtitle:
Firmware for serial vacuum subbase (VBL)
Description:

Supported systems:VABX-A-S-VE-BH-VBxxL

  • Valve terminal VTUX-A-S- (8000805)
  • Valve terminal VTUX-A-S-APA- (8000815)
  • Subbase VABX (8000870)
Document type:
Firmware
Version Download
Version 1.7.3
  • Bug fix switching behavior for installed NQ valve in error air saving condition. (KV valves are not affected)
  • New (higher) levels for overvoltage diagnosis
  • Firmware support for HW version 1 and 2
Version 1.7.1
  • General bug fixing
  • Improved error-handling process quality
Version 1.6.13
  • Support display module 
  • General bug fixing
  • Saving parameters locally - Bug fix of V1.6.10 so that it no longer needs to be executed twice
  • Text in APDD exteded
  • Optimization holding current

 

To perform a firmware update of the existing modules to the new version, the AP main devices (masters) must be updated to at least the following version (or higher):

AP-I-EP: v1.7.4

AP-A-EP: v1.7.4

AP-A-EC: v1.8.4

AP-I-EC: v1.8.4

AP-A-PN: v1.5.14

AP-I-PN: v1.5.14

Version 1.5.4
  • Correction of the process data format (especially relevant for the actual vacuum value): LSB/MSB swapped. Please note, there is a break compared to the previous version, FW0.3.16.
  • General bug fixing
  • Simplifying the teaching process. See manual for details.
Version 0.3.16
  • Initial version for product relese