The device description of an AP device (APDD) is installed, updated or uninstalled in the backstage section of the Festo Automation Suite under ‘Repositories’ in the ‘AP Devices’ view. This is possible even if the connection to the AP device is disconnected.


Search field
2
Selected APDD
3
Details
4
Search button

Found APDDs
The buttons are only visible if no APDDs are installed.
|
Symbol |
Function |
|---|---|
![]() |
To search for device description files for AP devices on APDDfinder. To do this, enter the manufacturer name, device name, part number or product name. If you are connected to the internet, the search will start automatically as soon as a search term is entered. |
|
Found devices |
The devices found are displayed with their variants. Clicking on a device displays the available APDD versions for the device.
|
![]() |
Checks for updates of installed APDD files. |
![]() |
To install an APDD file from a local file directory. |