Adorners provide additional information for parameters. Hover the mouse pointer over the adorner to display it. The content and functionality of the adorner depend on the parameter.


Adorner

Status

Parameter name

Close

Parameter ID and data type

Description of the parameter

Command section with button
Command section
Some adorners have buttons for directly changing a parameter value. Clicking the relevant button transfers the value to the output or input field.
|
Button |
Function |
|---|---|
|
‘Default’ |
Sets the module parameter to the displayed default value. |
|
‘Maximum’ |
Sets the module parameter to the displayed maximum value. |
|
‘Minimum’ |
Sets the module parameter to the displayed minimum value. |
|
‘Last saved’ |
Sets the module parameter to the last value saved in the project. |
Status of device parameters
The current state of the device parameters is displayed as information, warning or error as follows:
-
Colour-coded identification of the adorner
-
Status icon
If the values of corresponding parameters are not consistent, the corresponding parameter panels can be opened with a button in the adorner.
|
Colour of the adorner |
Symbol |
Status |
Function |
|---|---|---|---|
|
Grey |
![]() |
Information |
Shows an information symbol, the title and the description of the affected parameter. The parameter is in the normal status. |
|
Orange |
![]() |
Warning |
Shows a warning symbol, the title and the description of the warning. The parameter can be written to the module. |
|
Red |
![]() |
Error |
Shows an error symbol, the title and the description of the error. The parameter cannot be written to the module. |
Structure of the parameter IDs
The parameter IDs consist of four components:
|
Components of a parameter ID |
Function |
|---|---|
|
P |
Identification P = parameter |
|
Number |
ID number of the parameter |
|
Instance |
Identifier for distinguishing similar parameters of several components, e.g.:
Example of parameter ID setpoint cycle time IO-Link master:
|
|
Index |
Identifier for the differentiation of similar parameters within an instance |
The ID number of the parameter, the instance and the index are separated by a dot.