The response of the modules can be parameterised in the working section of the context ‘Parameterization’. If the working section has the ‘Navigation’ sidebar, the available content panels of the current context can be selected there. With terminals, for example, the device configuration of the terminal can be edited manually on the ‘Terminal’ panel.
Some modules can be configured in different variants, e.g. to operate them with a special process data length. The selected variant is taken into account when exporting the project data.
The title bar of the working section shows the module name on the left-hand side and commands for the current content panel on the right-hand side.
|
Symbol |
Meaning |
Function |
|---|---|---|
![]() |
Save parameters permanently on the device |
Only active with an active connection: permanently saves changed parameter values in the device. |
![]() |
Copy parameters |
Copies the parameters of the selected module to the clipboard. |
![]() |
Insert parameters |
Inserts the parameter values from the clipboard into an identical module. |
![]() |
Import module configuration |
Loads the configuration for the selected module from the user computer. |
![]() |
Export module configuration |
Saves the configuration of the selected module to the user computer as a JSAN file. This configuration can be imported into the current project or a different project. |
![]() |
Undock |
Open the contents in a new window. |