The terminal acts as a bracket and mirrors the structure of the remote I/O system. The ‘Terminal’ panel shows a graphic and a table view of the current device configuration of the remote I/O system.
If module is not selected in the graphic view or the table view, the right sidebar shows the ‘Module Catalog’. If a module is selected, the right sidebar shows the ‘Overview’ view with additional information on the module.


Navigator

Table display of the device configuration

Graphic view of the device configuration

Module catalogue

AP address
If an AP master has been configured for the system, the AP addresses of the modules are calculated and displayed in the graphic view and in the first column of the table view. If AP addresses are not displayed, calculation is not possible.
The names in the table view can be edited. The names are saved as part of the project data when saving the project ⮫ Change module name.