<?xml version="1.0" encoding="utf-8"?><PCNbody xmlns:xsd="http://www.w3.org/2001/XMLSchema" xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance" xmlns="http://www.smartpcn.org/images/files/VDMA24903Schema/PCNbody"><masterData pcnFormatVersion="SmartPCN_3.08"><pcnNumber>000000289301</pcnNumber><pcnTitle>DGC(I)-25(-KF/-FA) - Insourcing of Guiding System</pcnTitle><pcnAlertType>Minor</pcnAlertType><pcnType>PCN</pcnType><pcnMfrName>Festo SE &amp; Co. KG</pcnMfrName><pcnProductCategory>DOCU</pcnProductCategory><pcnIssueDate>2025-10-06</pcnIssueDate><pcnAddInfo> -</pcnAddInfo><pcnRevision>2</pcnRevision><contacts><contact pcnContactType="Manufacturer"><pcnCustomerNumber> -</pcnCustomerNumber><pcnDunsNumber>123456789</pcnDunsNumber><pcnBusinessUnit> -</pcnBusinessUnit><pcnCompany>Festo SE &amp; Co. KG</pcnCompany><pcnEmail>productchange@festo.com</pcnEmail><address><pcnStreet>Ruiter Straße 82</pcnStreet><pcnZipCode>73734</pcnZipCode><pcnCity>Esslingen</pcnCity><pcnCountry>DE</pcnCountry></address></contact></contacts></masterData><difference><pcnChangeTitle>DGC(I)-25(-KF/-FA) - Insourcing of Guiding System</pcnChangeTitle><pcnChangeDetail>Reason of change:
The guide system (consisting of guide rail and roller carriages) is being modified 
for the DGC-25(-KF/-FA) pneumatic linear actuator.
This is due to the insourcing of the guide system, which was previously purchased as 
a third-party component.

Technical changes:
The change affects the guiding module consisting of carriages and guiding rail.
This change results in a minor modification of the visual appearance of the 
actuator (changed geometric properties of carriages and guiding rail, changed 
material and color of guiding rail), but has no impact on the functionality, 
interface or installation 
dimensions.
Due to the changed geometric properties of the rails and carriages, new spare parts 
are required; the spare parts carriages for the previous and future guide systems 
are not compatible. The spare parts for the different versions can be found in the 
spare parts catalog as soon as they are available.
</pcnChangeDetail><pcnRiskAssessment> -</pcnRiskAssessment><pcnFirstDelivery>2026-04-01</pcnFirstDelivery><pcnFeedbackUntil>2026-04-01</pcnFeedbackUntil><pcnChangeIdentificationMethod>- Changed geometric properties of the rails and carriages (see pictures)
- Changed rail material and color:
    - old version: stainless steel (silver)
    - new version: Tempered steel, burnished (black)</pcnChangeIdentificationMethod><pcnEffectiveDate>2026-04-01</pcnEffectiveDate></difference><ItemNumbers><ItemNumber><itemMfrNumber>000000000000532447</itemMfrNumber><itemMfrTypeIdent>DGC-25-    -</itemMfrTypeIdent><itemMfrName>Linear drive    DGC-25-    -</itemMfrName><itemCategory>RAWM</itemCategory><itemLifeCycleData itemEOPeffDate="2026-04-01" /><itemChanges><itemChange itemChangeType="FORM"><itemChangeText>FORM</itemChangeText></itemChange><itemChange itemChangeType="CHARA"><itemChangeText>DGC</itemChangeText></itemChange></itemChanges></ItemNumber><ItemNumber><itemMfrNumber>000000000000544426</itemMfrNumber><itemMfrTypeIdent>DGCI-25-    -</itemMfrTypeIdent><itemMfrName>Linear drive    DGCI-25-    -</itemMfrName><itemCategory>RAWM</itemCategory><itemLifeCycleData itemEOPeffDate="2026-04-01" /><itemChanges><itemChange itemChangeType="FORM"><itemChangeText>FORM</itemChangeText></itemChange><itemChange itemChangeType="CHARA"><itemChangeText>DGCI</itemChangeText></itemChange></itemChanges></ItemNumber></ItemNumbers><pcnLifeCycleData><pcnSOP>2026-04-01</pcnSOP><pcnEOS>2026-04-01</pcnEOS><pcnEOPeffDate>2026-04-01</pcnEOPeffDate><pcnLTD>2026-04-01</pcnLTD><pcnEOSR>2026-04-01</pcnEOSR></pcnLifeCycleData></PCNbody>