The ‘Command Line’ panel in the ‘Diagnosis’ context enables advanced applications to read and write parameter values in a command line, ⮫ Working with the command line.

|
Window section |
Function |
|---|---|
|
‘Process Data’ |
Displays the process data of the inputs and outputs of the device in hexadecimal notation. The process data are automatically read when the panel is opened. Process data can also be saved in the device. |
|
‘Parameter’ |
Displays the values of parameters in hexadecimal notation. Parameter values can also be saved in the device. |
|
‘Timestamp’ |
Displays the read or write operations performed in the current session of the plug-in with timestamp and response from the device:
|

parameter value was successfully read or saved in the device
parameter value could not be read or saved in the device, or is not available in
the device.