The ‘Parameterization’ context includes the following panels:
|
Page |
Function |
|---|---|
|
‘Device’ |
If a device is connected: displays the device configuration, its identification data and the active user role ⮫ Device panel. |
|
‘Connection’ |
If a device is connected: shows the wiring and pin allocation of the device and a corresponding description, ⮫ Connection panel. |
|
‘Process Data’ |
If a device is connected: displays the device process data and enables forcing of values, ⮫ Process data panel. |
|
‘Device Control’ |
To execute the commands supported by the device, ⮫ Device control panel. |
|
‘IO-Link’ |
Displays the version of the IODD file and the physical communication data of the device, ⮫ IO-Link panel. |
|
‘Parameter List’ |
Shows the device parameters. Depending on the user role, which is set in ‘Device’, the modifiable parameter values can be changed and sent to the device or simply displayed, ⮫ Parameter list panel. |