﻿____________________________________________________________________________________________________

Version: 1.3.1.1

Fixed Bugs:

  •  Updating parameter values (Refresh Button) in the parameter list causes a plug-in crash for certain devices.
____________________________________________________________________________________________________

Version: 1.3.0.2

New Features:
	• Extended Parameter List Actions
          The parameter list has been extended with action buttons that can now be triggered directly from the parameter list.
	• Live Mode for Traces
          A live mode for traces has been added, allowing trace data to be collected live from the device.
	• Virtual Assistant Integration
          The virtual assistant has been integrated into the right sidebar of the plug-in.
	• Dedicated Backup & Restore Button
          Backup & Restore can now be triggered using one dedicated button.
Fixed Bugs:
	• Plug-in Crash with Certain IO-Link Devices
          An issue has been fixed where the plug-in crashed when used with certain IO-Link devices.
	• Plug-in Could Not Be Opened with Certain IO-Link Devices
          An issue has been fixed where the plug-in could not be opened when certain IO-Link devices were used.
	• Plug-in Crash During Blocked Parameter Write Access
          An issue has been fixed where the plug-in crashed when parameter write access was blocked.
____________________________________________________________________________________________________

Version: 1.2.1.22

Fixed Bugs:

  •  Sporadic plug-in crash when acknowledging device errors in the menu bar
  •  Incorrect or inverted display when forcing process data
  •  Plug-in crash when forcing outputs on the Process Data page for certain devices
____________________________________________________________________________________________________

Version: 1.2.0.275

New Features:
  •  Support for IO-Link devices with IODD standard V1.0
  •  Convenient display of live values in online mode in the right sidebar
  •  Custom configuration of the watchlist by individually adding device parameters
  •  Easy toggling of cyclical and acyclical device communication
  •  Configurable recording duration and automatic termination of trace recording

Fixed Bugs:
  •  Parameter values out of range of the data type lead to an inconsistent project in some devices (e.g., VPPM).
  •  Establishing a connection to devices is partially not possible due to the "timeout" being set too low.
  •  The plug-in cannot be opened if the included IODD is not installed in the project.
  •  Trace recordings are sporadically not displayed after reading out.
  •  Connection to the device is partially not possible when devices are added later from the scan pop-up.
  •  Incorrect interpretation of the Boolean data type leads to inverted parameter values in some devices.
____________________________________________________________________________________________________

Version: 1.1.1.1

Fixed Bugs:

  •  Parameter values that are transferred to the device are reset to the initial value after a few seconds.
____________________________________________________________________________________________________

Version: 1.1.0.153

New Features:

  •  Easy configuration and trace recording from data of IO-Link devices, e.g. monitoring of connected devices, in context Diagnosis
  •  Extended Trace display page for analyzing recorded traces with convenient features like, Zoom in/out, hide and show channels, combing axes etc.
  •  Start and Stop trace recordings easily via its own button in the ribbon bar
  •  Generic In- and output of Index and Subindex for e.g. process data of IO-Link device through an integrated command line view
  •  Desired IODD-version can be selected very comfortable on the plug-in page IO-Link (in case of several IODD-files)

Fixed Bugs:

  •  Live values of the device are updated very slow in online mode
  •  Process data from IO-Link devices cannot be written via CPX-AP-A IO-Link master
____________________________________________________________________________________________________

Version: 1.0.0.219

New Features:

  •  Parameterization and configuration of all IO-Link Devices with revision V1.1
  •  Dynamically displaying of parameter pages and its content depending on the loaded IODD device description
  •  Forces of process data possible when the plug-in is connected to the device
  •  Incoming device events and diagnosis messages are shown in the Plug-in context "Diagnosis"
  •  Device actions like e.g. Reset to factory or acknowledge error can be executed on a designed page "Device Control"
  •  Additional parameter information, a short description and the default value is available in pop up of each parameter (gray square)
  •  All device parameters are shown in a generic parameter list and can be filtered
  •  Helpful explanation regarding the plug connection and wiring are shown on page "Connection"
  •  Imported IODD device descriptions are stored in the project file and can be loaded on other systems
  •  Special device information and e.g. manuals are easily and conveniently accessible via the right sidebar (only for Festo devices)

Known Limitations:

  •  IO-Link Device with Revision V1.0 are not supported yet.