The display of the parameter values and the input options depends on the data type. The following data types are used:
|
Type |
Display in a parameter list |
|
|---|---|---|
|
Numerical values |
Input box |
![]() |
|
Boolean expression (activated or deactivated) |
Checkbox |
![]() |
|
Values lists of parameters |
List |
![]() |
-
Open the ‘Parameter List’ panel or another panel with parameters in the navigator.
-
Change the parameter value and confirm with Enter or move the cursor to another field. Alternatively, click the ‘Update’ button for the parameter group or ‘Update All’ at the top of the page.
If a connection is established to the device, the new parameter value is immediately active in the device.
If the device is not connected, the new parameter value is saved in the project. The parameter values will be synchronised next time the device is connected. ⮫ Synchronised data.