The right sidebar shows the following information about a selected device:
|
Range |
Function |
|---|---|
|
Watch list |
Parameter assignment for the current device description (IODD); the parameters are displayed in black, the values in blue. Use the |
|
Device properties |
Device code, order text, part number If the device is not yet connected, initial values are displayed. If the device is already connected, the data read from the device are saved together with the project and displayed whether the device is connected or not. |
|
Support information |
Documents and files relating to the Festo IO-Link devices, user manuals, application notes, device description files Documents and files for Festo IO-Link devices can be downloaded and displayed for support with the ‘Open Document’ button. Files that have already been downloaded can be accessed offline. |
|
Virtual assistant |
Access to the Festo virtual assistant. After logging into the MyFesto account, the virtual assistant in the form of a chatbot provides information on products and their installation, assembly, maintenance and fault clearance. |

button to edit the watchlist. This is only possible if the maximum number of parameters
in