Adorners provide additional information for parameters. Hover the mouse pointer over the adorner to display it. Content and functionality depend on the parameter.


Adorner

Status

Parameter name

Parameter with index and subindex, data format in brackets

Description of the parameter

Command section with mouse-over buttons

Copy information to the clipboard
Command section
Some adorners have buttons for directly changing a parameter value. Clicking the relevant button transfers the value to the output or input field.
|
Button |
Function |
|---|---|
|
‘Minimum’ |
Resets the device parameter to the displayed minimum value. |
|
‘Maximum’ |
Sets the device parameter to the displayed maximum value. |
|
‘Default’ |
Sets the device parameter to the displayed default value. |
|
‘Recomm. minimum’ |
Resets the device parameter to the displayed recommended minimum value. |
|
‘Recomm. maximum’ |
Sets the device parameter to the displayed recommended maximum value. |
|
‘Last saved’ |
Sets the device parameter to the most recently saved value in the project. |
Status of device parameters
The current state of the device parameters is displayed as information, warning or error as follows:
-
Colour-coded identification of the adorner
-
Status icon in the pop-up
If the values of corresponding parameters are not consistent, the corresponding parameter panels can be opened with a button in the adorner.
|
Colour of the adorner |
Symbol |
Status |
Function |
|---|---|---|---|
|
Grey |
![]() |
Information |
Shows an information symbol, the title and the description of the affected parameter. The parameter is in the normal status. |
|
Orange |
![]() |
Warning |
Shows a warning symbol, the title and the description of the warning. The parameter can be written to the device. |
|
Red |
![]() |
Error |
Shows an error symbol, the title and the description of the error. The parameter cannot be written to the device. |