The ‘Diagnosis’ context includes the following panels:
|
Page |
Function |
|---|---|
|
‘Device State’ |
If a device is connected: displays the current diagnostics events of the device, ⮫ Device status panel. |
|
‘Trace Configuration’ |
Displays the parameters and settings to for configuration of the recording ⮫ Trace settings panel. |
|
‘Trace Display’ |
Displays the retrieved trace data. The trace data can be analysed and exported ⮫ Trace display panel. |
|
‘Command Line’ |
Read and write parameter values for advanced applications on a command line, ⮫ Command line panel. |